LPC4370 Single cycle Multiply

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4370 Single cycle Multiply

10,221 Views
cpchen
Contributor II

Dear Sir,  

I like to use the single cycle multily capability of LPC4370 M4 core,   can you advise what should I do speicifically for this ? in code or in compiler ?

Best Regards,

Labels (1)
0 Kudos
Reply
10 Replies

10,026 Views
converse
Senior Contributor V

If you use a compiler, and a multiply in your code (i.e. a = b * c), it will automatically use the correct single cycle multiply instruction. There is no need to write it by hand.

0 Kudos
Reply

10,026 Views
cpchen
Contributor II

Hi Con Verse, 

THanks for the reply.  I am first time with Cortex M4 and LPC4370,  could you advise following clarification 

1. Do I need to define FPU exitence or include certain h file before compilier can automatically generate the correct single cycle multiplt istruction

2. Is there any way I can verify the compiled assembly code, I am useing MCUExpresso 

3. Have you use the FPU before, what's the processor you use ?

THansk for help !

0 Kudos
Reply

10,027 Views
converse
Senior Contributor V

1. Single cycle multiply (integer) is nothing to do with FPU (floating point). No, you don't need to do anything. Just write your code.

2. What, don't you trust the compiler? You can generate assembly output if you want to see what is generated. See https://mcuoneclipse.com/2018/07/08/creatin… 

3. Yes, I use FPU. DOn't forget it is single precision (32-bit, or 'float' in C). If you use double precision in your code ('double' in C), then it is emulated, so it will be slow. Take a look at this https://mcuoneclipse.com/2018/07/08/creatin… 

Also, make sure you read section 19.4 (Floating point support) in the latest MCUXpresso IDE User Guide. 

0 Kudos
Reply

10,027 Views
cpchen
Contributor II

Hi Con Verse, 

I just found out both links you provide above is not exist anymore, is there any other place I can see the article ?

pastedImage_1.png

0 Kudos
Reply

10,027 Views
converse
Senior Contributor V
0 Kudos
Reply

10,026 Views
cpchen
Contributor II

Thanks , appreciated !

0 Kudos
Reply

10,026 Views
cpchen
Contributor II

Thanks a lot for the reply. it's very helpful.  

I mix single cycle multiply with FPU,  what I need in my application is multiply with floating numbers, I will look into it. 

Thanks again !

0 Kudos
Reply

10,023 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Chen,

If you would like to get single cycle multiply operation, I suppose that you can use the assembly language to finish the job in order to maximize the effiency. I attach the Cortex-M4 generic user guide, which includes the assembly instruction of the core. You can develop project in C language, you can declare an api function and implement the body of the api function with assembly language, there is calling convention for api function based compiler, but it is compiler by compiler.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply

10,023 Views
cpchen
Contributor II

Got  the attachment, thank you !

0 Kudos
Reply

10,022 Views
cpchen
Contributor II

Hi Xiangjun, 

Thank you for the reply, I did not see the attachment,  can you send it again ?

Best Regards,

0 Kudos
Reply