LPC4370(SPIFI Boot) Debug and Download Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4370(SPIFI Boot) Debug and Download Problem

1,982 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by park957 on Mon May 26 05:48:27 MST 2014
hi,

I use LPC4370 + SPIFI Boot (SPANSION S25FL032) + ULINK2 + KEIL4.

There is one problem, RAM Debug is OK.

but, SPIFI Download and Debug is Problem...



[img]http://img2.ruliweb.daum.net/mypi/gup/a/58/4/o/3188080950.jpg[/img]
[img]http://img2.ruliweb.daum.net/mypi/gup/a/58/4/o/3188080951.jpg[/img]
[img]http://img2.ruliweb.daum.net/mypi/gup/a/58/4/o/3188080952.jpg[/img]
[img]http://img2.ruliweb.daum.net/mypi/gup/a/58/4/o/3188080953.jpg[/img]
[img]http://img2.ruliweb.daum.net/mypi/gup/a/58/4/o/3188080954.jpg[/img]
[img]http://img2.ruliweb.daum.net/mypi/gup/a/58/4/o/3188080965.jpg[/img]




Does someone know how I can solve this problem?



标签 (1)
0 项奖励
回复
3 回复数

1,936 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by park957 on Tue May 27 17:51:52 MST 2014

Thanks for the quick reply NXP Support.

I solved the problem well.

My critical mistake was the wrong ini file was used.

And the wrong util page setting.

Thank you~ NXP~

0 项奖励
回复

1,936 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Tue May 27 14:35:37 MST 2014
Hi Park957,
Could you please put device in to ISP mode and then try to erase device and download firmware after that?
0 项奖励
回复

1,936 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Mon May 26 08:56:31 MST 2014
Don't send an init file for the flash utilitiy, just for the debugger.
As RAM debug works there is no generic problem for the debugger to get access to the ARM core, so the wrong setting for this init file is the only reason I could think of.

Regards,
NXP Support Team
0 项奖励
回复