LPC4370 M0SUB core Jtag access accidentally disabled

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4370 M0SUB core Jtag access accidentally disabled

ソリューションへジャンプ
3,505件の閲覧回数
zhengyangqu
Contributor II

I encountered the same problem as mentioned in this thread.

 BUT I found something interesting. Hope someone can solve the problem.

lpcscrypt.exe queryOTPMem

0x40045000 200000e0 00724f66 143905b3 00408187
0x40045010 00000000 00000000 00000000 00000000
0x40045020 00000000 00000000 00000000 00000000
0x40045030 20000080 00400000 00000000 00408000
0x40045040 00000000 00000000 00000000 00000000
0x40045050 83d9a706 9ec0e9d3 52ed8912 d44f2a3e
0x40045060 00000000 00000000 00000000 00000000
0x40045070 00000000 00000000 00000000 00000000

lpcscrypt.exe querypartdetailed

partID = 0x200000e0 0
decode = LPC43S70: - No Internal Flash
Core Clock = 180000000
Decoding: b100000000000000000000011100000
0:1 b00 USB0 USB2.0 HS
2:3 b00 USB1 USB2.0 HS (extern ULP)
4:6 b110 AES Capable
7 b1 CAN0 Disabled
8 b0 ETH Enabled
9 b0 LCD Enabled
10 b0 TURBO Capable
11 b0 M0sub Enabled
12 b0 M0app Enabled
13 b0 CAN1 Enabled
14 b0 SRAM_DATA 72KB at 0x10080000
15:16 b0 SRAM_CODE 128KB at 0x10000000
17 b0 SRAM_USB 32KB at 0x20000000
18 b0 SRAM_ETB 16KB at 0x2000c000
19 b0 SRAM_ETH 16KB at 0x20008000
20:26 Reserved
27 b0 EZH Enabled
28 b0 SGPIO Enabled
29 b1 M0sub_JTAG Disabled
30 b0 M0app_JTAG Enabled
31 b0 VADC Enabled
0 件の賞賛
返信
1 解決策
3,251件の閲覧回数
zhengyangqu
Contributor II

According to this errata - 3.12 OTP.2, LPC4370 sometimes erroneously programs OTP memory. Some bits inside OTP will surely disable debug access to certain cores.

Should use special circuit to avoid this problem.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,252件の閲覧回数
zhengyangqu
Contributor II

According to this errata - 3.12 OTP.2, LPC4370 sometimes erroneously programs OTP memory. Some bits inside OTP will surely disable debug access to certain cores.

Should use special circuit to avoid this problem.

0 件の賞賛
返信
3,251件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Zhengyang,

   Do you modify the OTP area by yourself on our board?

  From your post information, your 0x40045030 is  0x20000080, is it LE mode or BE mode? If BE mode, your JTAG_DISABLE bit is set, then the JTAG cann't be enabled by software and remains disabled.

pastedImage_2.png

Do you configure the OTP area by yourself?

Besides, do you try to use the Cortex M4 to read it, is it the same result?


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,251件の閲覧回数
zhengyangqu
Contributor II

Thanks for your reply, Kerry.

Do you modify the OTP area by yourself on our board?

No, I was developing when finding M0SUB unaccessible.

is it LE mode?

Yes, it's LE mode, but 0x20000080 = 0b0010'0000'0000'0000'0000'0000'1000'0000 , bit31 is not set. but reserved bit 29 is set.

Do you configure the OTP area by yourself?

No.

Besides, do you try to use the Cortex M4 to read it, is it the same result?

Yes, I got this result with LPCScrypt software provided by NXP.

Besides, I found CREG5 is 0xc0000660 after reset. Bit 10 M0SUBTAPSEL is always set.

0 件の賞賛
返信
3,251件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Zhengyang Qu,

    Thanks a lot for your updated information.

    It's my mistake, yes, you are correct, if it is the LE mode, the JTAG_DISABLE bit is enabled.

   I also check the OTP memory, this is my LPC-LINK2 information:

pastedImage_1.png

  Yes, your JTAG_DISABLE is still enabled, about the reserved bit, we can ignore the data.

  I have a question, if you the JLINK commander with SWD interface or JTAG interface, do you can connect your Cortext M4 core?

pastedImage_2.png

pastedImage_3.png


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,251件の閲覧回数
zhengyangqu
Contributor II

Thanks for your reply, Kerry.

This is my result.

微信截图_20180719154734.png

微信截图_20180719155059.png

I have M4 and M0APP cores access.

PS: On another board with M0SUB core access, the result shows 3 JTAG taps can be detected. I think your LINK2 may have the same problem.

微信截图_20180719155239.png

0 件の賞賛
返信