LPC4370 High Speed ADC initial delay.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4370 High Speed ADC initial delay.

2,173件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mshrestha789 on Tue Nov 03 10:56:12 MST 2015
Hello friends,

Recently I have been working on High speed ADC of the LPC4370 microcontroller. I need to detect the threshold and then capture the data, I managed to do that however, many times ADC misses certain data at the beginning. I attached here the screeshot of the captured data and part of ADC code. This behavior very random. Please help me regarding this.

void adc_init(void){
Chip_Clock_SetDivider(CLK_IDIV_A, CLKIN_USBPLL, 2); // USB clock 480 MHz -> CLKIN_IDIVA = 480/2=240
Chip_Clock_SetDivider(CLK_IDIV_B, CLKIN_IDIVA, 3);  // CLCIN_IDIVB = CLKIN_IDIVB = 240/3 = 80
Chip_Clock_SetBaseClock(CLK_BASE_ADCHS, CLKIN_IDIVB, true, false);


Chip_Clock_EnableOpts(CLK_ADCHS, true, true, 1);
Chip_HSADC_Init(LPC_ADCHS_CMSIS);


Chip_HSADC_SetupFIFO(LPC_ADCHS_CMSIS, 8, true);
Chip_HSADC_ConfigureTrigger(LPC_ADCHS_CMSIS, HSADC_CONFIG_TRIGGER_SW, HSADC_CONFIG_TRIGGER_RISEEXT, HSADC_CONFIG_TRIGGER_NOEXTSYNC, HSADC_CHANNEL_ID_EN_ADD, 0x90);


Chip_HSADC_SetACDCBias(LPC_ADCHS_CMSIS, 0, HSADC_CHANNEL_NODCBIAS, HSADC_CHANNEL_NODCBIAS);

Chip_HSADC_SetThrLowValue(LPC_ADCHS_CMSIS, 0, 10);
Chip_HSADC_SetThrHighValue(LPC_ADCHS_CMSIS, 0, 3000);

Chip_HSADC_SetPowerSpeed(LPC_ADCHS_CMSIS, false);
Chip_HSADC_EnablePower(LPC_ADCHS_CMSIS);

Chip_HSADC_SetupDescEntry(LPC_ADCHS_CMSIS, 0, 0, (HSADC_DESC_CH(0) | HSADC_DESC_THRESH_A | HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(HSADC_DESCRIPTOR_TIME) | HSADC_DESC_RESET_TIMER));
Chip_HSADC_SetupDescEntry(LPC_ADCHS_CMSIS, 0, 1, (HSADC_DESC_CH(0) | HSADC_DESC_THRESH_A | HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(HSADC_DESCRIPTOR_TIME) | HSADC_DESC_RESET_TIMER));
Chip_HSADC_SetupDescEntry(LPC_ADCHS_CMSIS, 0, 2, (HSADC_DESC_CH(0) | HSADC_DESC_THRESH_A | HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(HSADC_DESCRIPTOR_TIME) | HSADC_DESC_RESET_TIMER));
Chip_HSADC_SetupDescEntry(LPC_ADCHS_CMSIS, 0, 3, (HSADC_DESC_CH(0) | HSADC_DESC_THRESH_A | HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(HSADC_DESCRIPTOR_TIME) | HSADC_DESC_RESET_TIMER));
Chip_HSADC_SetupDescEntry(LPC_ADCHS_CMSIS, 0, 4, (HSADC_DESC_CH(0) | HSADC_DESC_THRESH_A | HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(HSADC_DESCRIPTOR_TIME) | HSADC_DESC_RESET_TIMER));
Chip_HSADC_SetupDescEntry(LPC_ADCHS_CMSIS, 0, 5, (HSADC_DESC_CH(0) | HSADC_DESC_THRESH_A | HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(HSADC_DESCRIPTOR_TIME) | HSADC_DESC_RESET_TIMER));
Chip_HSADC_SetupDescEntry(LPC_ADCHS_CMSIS, 0, 6, (HSADC_DESC_CH(0) | HSADC_DESC_THRESH_A | HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(HSADC_DESCRIPTOR_TIME) | HSADC_DESC_RESET_TIMER));
Chip_HSADC_SetupDescEntry(LPC_ADCHS_CMSIS, 0, 7, (HSADC_DESC_CH(0) | HSADC_DESC_THRESH_A | HSADC_DESC_BRANCH_SWAP | HSADC_DESC_MATCH(HSADC_DESCRIPTOR_TIME) | HSADC_DESC_RESET_TIMER));

Chip_HSADC_SetupDescEntry(LPC_ADCHS_CMSIS, 1, 0, (HSADC_DESC_CH(0) | HSADC_DESC_THRESH_A | HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(HSADC_DESCRIPTOR_TIME) | HSADC_DESC_RESET_TIMER));
Chip_HSADC_SetupDescEntry(LPC_ADCHS_CMSIS, 1, 1, (HSADC_DESC_CH(0) | HSADC_DESC_THRESH_A | HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(HSADC_DESCRIPTOR_TIME) | HSADC_DESC_RESET_TIMER));
Chip_HSADC_SetupDescEntry(LPC_ADCHS_CMSIS, 1, 2, (HSADC_DESC_CH(0) | HSADC_DESC_THRESH_A | HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(HSADC_DESCRIPTOR_TIME) | HSADC_DESC_RESET_TIMER));
Chip_HSADC_SetupDescEntry(LPC_ADCHS_CMSIS, 1, 3, (HSADC_DESC_CH(0) | HSADC_DESC_THRESH_A | HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(HSADC_DESCRIPTOR_TIME) | HSADC_DESC_RESET_TIMER));
Chip_HSADC_SetupDescEntry(LPC_ADCHS_CMSIS, 1, 4, (HSADC_DESC_CH(0) | HSADC_DESC_THRESH_A | HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(HSADC_DESCRIPTOR_TIME) | HSADC_DESC_RESET_TIMER));
Chip_HSADC_SetupDescEntry(LPC_ADCHS_CMSIS, 1, 5, (HSADC_DESC_CH(0) | HSADC_DESC_THRESH_A | HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(HSADC_DESCRIPTOR_TIME) | HSADC_DESC_RESET_TIMER));
Chip_HSADC_SetupDescEntry(LPC_ADCHS_CMSIS, 1, 6, (HSADC_DESC_CH(0) | HSADC_DESC_THRESH_A | HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(HSADC_DESCRIPTOR_TIME) | HSADC_DESC_RESET_TIMER));
Chip_HSADC_SetupDescEntry(LPC_ADCHS_CMSIS, 1, 7, (HSADC_DESC_CH(0) | HSADC_DESC_THRESH_A | HSADC_DESC_INT | HSADC_DESC_BRANCH_SWAP | HSADC_DESC_MATCH(HSADC_DESCRIPTOR_TIME) | HSADC_DESC_RESET_TIMER));

Chip_HSADC_UpdateDescTable(LPC_ADCHS_CMSIS, 0);
Chip_HSADC_UpdateDescTable(LPC_ADCHS_CMSIS, 1); 
}

static void vadc_control_task(void *pvParameters){
while (1) {
if(xSemaphoreTake(g_adc_trigger, 10)== pdTRUE){ //wait for trigger
Chip_HSADC_SetActiveDescriptor(LPC_ADCHS_CMSIS, 0, 0); // set active descriptor
Chip_HSADC_SWTrigger(LPC_ADCHS_CMSIS); //software trigger
while((Chip_HSADC_GetLastSample(LPC_ADCHS_CMSIS, 0) & HSADC_LS_RANGE_ABOVE) != HSADC_LS_RANGE_ABOVE); //wait for threshold
Chip_HSADC_FlushFIFO(LPC_ADCHS_CMSIS);
LPC_GPDMA->C0CONFIG  |=  (0x1); //initialize DMA transfer
while(1){
if(LPC_GPDMA->INTTCSTAT & (((1UL << 0) & 0xFF))){
break;
}
}

}
}
ラベル(1)
0 件の賞賛
返信
1 返信

1,960件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mshrestha789 on Thu Nov 05 01:38:08 MST 2015
Hi,

Is there any chance its because of DMA transfer?

Recently I disable the DMA synchronization with LPC_GPDMA->SYNC = 0x01, it improved the performance. However, it still misses some data sometime.

Please help me regarding this.
0 件の賞賛
返信