LPC4370 HSADC external VIN_NEG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4370 HSADC external VIN_NEG

1,241 Views
colinstephant
Contributor I


Hi,

I'm using a LPC4370 HSADC wich is working good with internal DC VIN_NEG reference.

Now I want to use the external reference wich is at  360mV on the board, but as soon as I execute Chip_HSADC_EnablePower(LPC_ADCHS) the VIN_NEG pin outputs 500mV.

Here is the code that we execute :

setupClock(frequency); // Configure clock for measure.

  Chip_HSADC_Init(LPC_ADCHS); // Initialize HSADC.

  Chip_HSADC_DisablePowerDownMode(LPC_ADCHS);

  Chip_HSADC_SetupFIFO(LPC_ADCHS, FIFO_INT_SIZE, PACKED_FIFO); // Configure FIFO.

  // Select negative as external reference, Positive as external.

  Chip_HSADC_SetACDCBias(LPC_ADCHS, currentChannel, HSADC_CHANNEL_NODCBIAS, HSADC_CHANNEL_NODCBIAS);

  for(i = 0; i < 1;i++)

  {

  Chip_HSADC_SetActiveDescriptor(LPC_ADCHS,0,i); // Activate descriptor table 0 with 0<ID<8.

  Chip_HSADC_SetupDescEntry(LPC_ADCHS, 0, i,0);

  }

  // External trigger only, on falling edge, 0x90 recovery clocks, add channel IF to FIFO entry

  Chip_HSADC_ConfigureTrigger(LPC_ADCHS, HSADC_CONFIG_TRIGGER_EXT,

  HSADC_CONFIG_TRIGGER_RISEEXT,

  HSADC_CONFIG_TRIGGER_NOEXTSYNC,HSADC_CHANNEL_ID_EN_ADD, 0x90);

  // Edge detection enabled/Synchronization/No pulse

  LPC_GIMA->ADCHS_TRIGGER_IN = (1 << 1 | 1 << 2 | 0 << 3 );

  // Only one PWM used as trigger source.

  LPC_GIMA->ADCHS_TRIGGER_IN |= 7 << 4; // CTOUT_8

  Chip_HSADC_SetupDescEntry(LPC_ADCHS,0, 0, (HSADC_DESC_CH(currentChannel) |

  HSADC_DESC_BRANCH_FIRST | HSADC_DESC_MATCH(1)| HSADC_DESC_THRESH_NONE |HSADC_DESC_RESET_TIMER ));

  Chip_HSADC_SetPowerSpeed(LPC_ADCHS,true);

  Chip_HSADC_EnablePower(LPC_ADCHS);

  Chip_HSADC_DisablePowerDownMode(LPC_ADCHS);


Any idea of what's happening ?

Labels (1)
1 Reply

951 Views
soledad
NXP Employee
NXP Employee

Hi,

Could you please try using the following configuration?

Chip_HSADC_SetACDCBias(LPC_ADCHS, 0, HSADC_CHANNEL_DCBIAS, HSADC_CHANNEL_NODCBIAS);

Please let me know if this helps.
Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------