LPC4370 GPDMA Transfer problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4370 GPDMA Transfer problem

ソリューションへジャンプ
2,226件の閲覧回数
aliasadzadeh
Contributor II

Hi,

I wanted to just make some timer triggered DMA transfers, using Timer3 MAT0 as the trigger, here is my sample code, but I do not know what's going on that the timer would not make any requests into the DMA, my code for memory to memory Would works just fine. there is no DMA transaction!!!!:smileysad:

#include "LPC43xx.h" // Device header
#include "GPDMA_LPC43xx.h" // Keil::Device:GPDMA
#include "GPIO_LPC43xx.h" // Keil::Device:GPIO
#include "SCU_LPC43xx.h" // Keil::Device:SCU

uint16_t SPITXDummi[8]={0x1234,2,3,4,5,6,122,145};
uint16_t SPIRXDummi[8];

int main(void)
{

/* Confige timer 3 to make request 500ms each since we use 180MHz Clock */
LPC_TIMER3->MR0=90000000;
/* interrupt on MR0, reset timer on match 0 */
LPC_TIMER3->MCR = 0x0003;
/* toggle MAT0.0 pin on match */
LPC_TIMER3->EMR = 0x0031;
/* Reset Timer */
LPC_TIMER3->TCR = 2;


//Select Timer3 MR0 as DMA Request
GPDMA_PeripheralSelect (7, 0);

LPC_GPDMA->CONFIG = 1;
LPC_GPDMA->INTTCCLEAR = 0xFFFFFFFF;
LPC_GPDMA->INTERRCLR = 0xFFFFFFFF;
/* Enable synchro logic request */
LPC_GPDMA->SYNC = 0;

LPC_GPDMA->C0SRCADDR = (uint32_t) &SPITXDummi[0];
LPC_GPDMA->C0DESTADDR = (uint32_t)&LPC_TIMER3->MR1;//(uint32_t) &SPIRXDummi[0];

LPC_GPDMA->C0LLI = 0; // linked lists for ch0
LPC_GPDMA->C0CONTROL = 8 // transfer size (0 - 11) = 32
| (0 << 12) // source burst size (12 - 14) = 1
| (0 << 15) // destination burst size (15 - 17) = 1
| (2 << 18) // source width (18 - 20) = 32 bit
| (2 << 21) // destination width (21 - 23) = 32 bit
| (1 << 24) // source AHB select (24) = AHB 0
| (1 << 25) // destination AHB select (25) = AHB 0
| (1 << 26) // source increment (26) = increment
| (0 << 27) // destination increment (27) = no increment
| (0 << 28) // mode select (28) = access in user mode
| (0 << 29) // (29) = access not bufferable
| (0 << 30) // (30) = access not cacheable
| (1 << 31); // terminal count interrupt

LPC_GPDMA->C0CONFIG = 1 // channel enabled (0)
| (7 << 1) // source peripheral (1 - 5) = none
| (0 << 6) // destination request peripheral (6 - 10) = MAT0.0
| (5 << 11) // flow control (11 - 13) = mem to per
| (0 << 14) // (14) = mask out error interrupt
| (0 << 15) // (15) = mask out terminal count interrupt
| (0 << 16) // (16) = no locked transfers
| (0 << 18); // (27) = no HALT


/* Reset Timer */
LPC_TIMER3->TCR = 2;
LPC_TIMER3->TCR = 1; // enable timer
while (LPC_GPDMA->C0CONFIG & 1);// wait for the DMA to finish
LPC_TIMER3->TCR = 0; // disable timer


while(1)
{

}
}

タグ(4)
0 件の賞賛
返信
1 解決策
1,978件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ali Asadzadeh

        About the LPC4370 GPDMA memory to memory transfer which is triggered by the timer match, actually, in our lpcopen code for LPC4370, the lpcxpresso IDE version, already have a sample code about it,  it is periph_dma_timertrig, you can refer to it, please download the lpcopen code from this link:

https://www.nxp.com/downloads/en/libraries/lpcopen_3_02_lpcxpresso_link2_4370.zip 

 This project is using the TIMER0, MATCH0 to trigger the DMA transfer, you can test it, after it works on your side, you can change the timer to timer3 match0.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,979件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ali Asadzadeh

        About the LPC4370 GPDMA memory to memory transfer which is triggered by the timer match, actually, in our lpcopen code for LPC4370, the lpcxpresso IDE version, already have a sample code about it,  it is periph_dma_timertrig, you can refer to it, please download the lpcopen code from this link:

https://www.nxp.com/downloads/en/libraries/lpcopen_3_02_lpcxpresso_link2_4370.zip 

 This project is using the TIMER0, MATCH0 to trigger the DMA transfer, you can test it, after it works on your side, you can change the timer to timer3 match0.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信