LPC4370 GPDMA Transfer problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC4370 GPDMA Transfer problem

跳至解决方案
2,217 次查看
aliasadzadeh
Contributor II

Hi,

I wanted to just make some timer triggered DMA transfers, using Timer3 MAT0 as the trigger, here is my sample code, but I do not know what's going on that the timer would not make any requests into the DMA, my code for memory to memory Would works just fine. there is no DMA transaction!!!!:smileysad:

#include "LPC43xx.h" // Device header
#include "GPDMA_LPC43xx.h" // Keil::Device:GPDMA
#include "GPIO_LPC43xx.h" // Keil::Device:GPIO
#include "SCU_LPC43xx.h" // Keil::Device:SCU

uint16_t SPITXDummi[8]={0x1234,2,3,4,5,6,122,145};
uint16_t SPIRXDummi[8];

int main(void)
{

/* Confige timer 3 to make request 500ms each since we use 180MHz Clock */
LPC_TIMER3->MR0=90000000;
/* interrupt on MR0, reset timer on match 0 */
LPC_TIMER3->MCR = 0x0003;
/* toggle MAT0.0 pin on match */
LPC_TIMER3->EMR = 0x0031;
/* Reset Timer */
LPC_TIMER3->TCR = 2;


//Select Timer3 MR0 as DMA Request
GPDMA_PeripheralSelect (7, 0);

LPC_GPDMA->CONFIG = 1;
LPC_GPDMA->INTTCCLEAR = 0xFFFFFFFF;
LPC_GPDMA->INTERRCLR = 0xFFFFFFFF;
/* Enable synchro logic request */
LPC_GPDMA->SYNC = 0;

LPC_GPDMA->C0SRCADDR = (uint32_t) &SPITXDummi[0];
LPC_GPDMA->C0DESTADDR = (uint32_t)&LPC_TIMER3->MR1;//(uint32_t) &SPIRXDummi[0];

LPC_GPDMA->C0LLI = 0; // linked lists for ch0
LPC_GPDMA->C0CONTROL = 8 // transfer size (0 - 11) = 32
| (0 << 12) // source burst size (12 - 14) = 1
| (0 << 15) // destination burst size (15 - 17) = 1
| (2 << 18) // source width (18 - 20) = 32 bit
| (2 << 21) // destination width (21 - 23) = 32 bit
| (1 << 24) // source AHB select (24) = AHB 0
| (1 << 25) // destination AHB select (25) = AHB 0
| (1 << 26) // source increment (26) = increment
| (0 << 27) // destination increment (27) = no increment
| (0 << 28) // mode select (28) = access in user mode
| (0 << 29) // (29) = access not bufferable
| (0 << 30) // (30) = access not cacheable
| (1 << 31); // terminal count interrupt

LPC_GPDMA->C0CONFIG = 1 // channel enabled (0)
| (7 << 1) // source peripheral (1 - 5) = none
| (0 << 6) // destination request peripheral (6 - 10) = MAT0.0
| (5 << 11) // flow control (11 - 13) = mem to per
| (0 << 14) // (14) = mask out error interrupt
| (0 << 15) // (15) = mask out terminal count interrupt
| (0 << 16) // (16) = no locked transfers
| (0 << 18); // (27) = no HALT


/* Reset Timer */
LPC_TIMER3->TCR = 2;
LPC_TIMER3->TCR = 1; // enable timer
while (LPC_GPDMA->C0CONFIG & 1);// wait for the DMA to finish
LPC_TIMER3->TCR = 0; // disable timer


while(1)
{

}
}

标记 (4)
0 项奖励
回复
1 解答
1,969 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ali Asadzadeh

        About the LPC4370 GPDMA memory to memory transfer which is triggered by the timer match, actually, in our lpcopen code for LPC4370, the lpcxpresso IDE version, already have a sample code about it,  it is periph_dma_timertrig, you can refer to it, please download the lpcopen code from this link:

https://www.nxp.com/downloads/en/libraries/lpcopen_3_02_lpcxpresso_link2_4370.zip 

 This project is using the TIMER0, MATCH0 to trigger the DMA transfer, you can test it, after it works on your side, you can change the timer to timer3 match0.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,970 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ali Asadzadeh

        About the LPC4370 GPDMA memory to memory transfer which is triggered by the timer match, actually, in our lpcopen code for LPC4370, the lpcxpresso IDE version, already have a sample code about it,  it is periph_dma_timertrig, you can refer to it, please download the lpcopen code from this link:

https://www.nxp.com/downloads/en/libraries/lpcopen_3_02_lpcxpresso_link2_4370.zip 

 This project is using the TIMER0, MATCH0 to trigger the DMA transfer, you can test it, after it works on your side, you can change the timer to timer3 match0.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复