LPC4370 - DMA P2M Too Much Data Transferred

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4370 - DMA P2M Too Much Data Transferred

2,892件の閲覧回数
rulamp
Contributor III

Hello,

I have DMA set up to move data from the HSADC FIFO to memory. This seems to work correctly, however there is some unexpected behavior.

The number of samples transferred is far larger than the 16 words expected. From my understanding, the DMA transfer is initiated when the HSADC FIFO_FULL flag is set. I have set the FIFIO fill level to 15. So after 15 samples, the DMA should trigger and move 16 samples out of the FIFO and into the destination address.

In the DMA handler, I reset the channel to get it ready for another transfer. From my understanding, the next time the DMA transfer occurs, the destination address should be the same (eg: dest[0]), however, it seems as though the destination address is the next address after the last transfer (eg: dest[16]).

This results in the DMA filling up memory incredibly rapidly.

What is going on here?

void DMA_IRQHandler(void)
{
	Chip_GPDMA_Interrupt(LPC_GPDMA, dmaCh); //clears it

	LPC_GPDMA->CH[dmaCh].SRCADDR = (uint32_t) &LPC_ADCHS->FIFO_OUTPUT[0];
	LPC_GPDMA->CH[dmaCh].DESTADDR = ((uint32_t) &dest[0]);
	LPC_GPDMA->CH[dmaCh].CONFIG |= 1;
}

void adchs_dma_setup(void)
{
	Chip_GPDMA_Init(LPC_GPDMA);

	dmaCh = Chip_GPDMA_GetFreeChannel(LPC_GPDMA, GPDMA_CONN_ADCHS_READ);

	Chip_GPDMA_Transfer(LPC_GPDMA, dmaCh,
					GPDMA_CONN_ADCHS_READ, (uint32_t) &dest[0],
					GPDMA_TRANSFERTYPE_P2M_CONTROLLER_PERIPHERAL,
					NULL);

	/* Enable GPDMA interrupt */
	NVIC_SetPriority(DMA_IRQn, 0);
	NVIC_ClearPendingIRQ(DMA_IRQn);
	NVIC_EnableIRQ(DMA_IRQn);
}

void adchs_setup(void)
{
	Chip_HSADC_Init(LPC_ADCHS);
	Chip_HSADC_SetupFIFO(LPC_ADCHS, 15, false);
	Chip_HSADC_ConfigureTrigger(LPC_ADCHS, HSADC_CONFIG_TRIGGER_SW,
			HSADC_CONFIG_TRIGGER_RISEEXT, HSADC_CONFIG_TRIGGER_NOEXTSYNC,
			HSADC_CHANNEL_ID_EN_NONE, 0x90);

	Chip_HSADC_SetACDCBias(LPC_ADCHS, 0, HSADC_CHANNEL_DCBIAS, HSADC_CHANNEL_NODCBIAS);
	Chip_HSADC_SetPowerSpeed(LPC_ADCHS, false);
	Chip_HSADC_EnablePower(LPC_ADCHS);
	Chip_HSADC_SetupDescEntry(LPC_ADCHS, 0, 0, (HSADC_DESC_CH(0) | HSADC_DESC_BRANCH_FIRST | HSADC_DESC_MATCH(1) | HSADC_DESC_THRESH_NONE | HSADC_DESC_RESET_TIMER));
	Chip_HSADC_EnableInts(LPC_ADCHS, 0, (HSADC_INT0_FIFO_FULL));
	Chip_HSADC_UpdateDescTable(LPC_ADCHS, 0);
	NVIC_EnableIRQ(ADCHS_IRQn);
}
0 件の賞賛
返信
5 返答(返信)

2,876件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you refer to the ticket?

https://community.nxp.com/t5/LPC-Microcontrollers/LPC4370-DMA-Issues/m-p/1636485#M52256

 

For the hsadc example in LPCopen, the ADC uses software  triggering, it can not reach up to 80MSPS.

Hope it can help you

BR

XiangJun Rong

 

0 件の賞賛
返信

2,865件の閲覧回数
rulamp
Contributor III

Hi XiangJun,

Maybe I am confused and do not understand you, but I think you might be confused and mixing up my question. I did not say anything in this post about 80MS/s. I did not say anything in this post about problems with the HSADC.
Yes, I understand that the example uses a software trigger executed in a timer interrupt. I am NOT asking about the example, though. I am asking about my code. As you can see in the descriptor entry, I branch to FIRST. This causes the ADC to run continuously. The works correctly.

My question is about DMA. My question is:
Why does the destination address continue to increment upon a new DMA transfer? The destination address should be dest[0], however, it is greater than dest[(16*num_of_transfers)].

Why is this happening? Again, I am NOT asking about ADC functionality.

0 件の賞賛
返信

2,843件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have checked your code, in the DMA_IRQHandler (), you reinitialize the LPC_GPDMA->CH[dmaCh].DESTADDR

with the line.

LPC_GPDMA->CH[dmaCh].DESTADDR = ((uint32_t) &dest[0]);

So, pls check if you have entered the DMA_IRQHandler ()

BR

XiangJun Rong

0 件の賞賛
返信

2,765件の閲覧回数
rulamp
Contributor III

Hello. Checking in to see if you have any other ideas as to the cause of the behavior?

0 件の賞賛
返信

2,836件の閲覧回数
rulamp
Contributor III

Hello,

Thank you for checking my code. Yes, I can confirm that my code enters, executes, and then exits the DMA_IRQHandler properly.

0 件の賞賛
返信