LPC4370 AND KEIL MDK VERSION 5 SERIES PROGRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4370 AND KEIL MDK VERSION 5 SERIES PROGRAM

2,924 Views
sujayp
Contributor II

Dear NXP Technical Support Services ,

 

I am writing in regards the programming for the LPC4370FET256 using the KEIL MDK ARM Version 5 using the Keil ULINK 2 debugger.

 

Since I couldn’t find the proper link for programming for the LPC4370FET256 using the KEIL MDK ARM Version 5 using the Keil ULINK 2 debugger.

 

I was having the link for the Keil MDK version 4.74 not the Keil MDK arm Ver 5 series which is a latest one software  in order to program the LPC4370FET256 from the external flash memory.

 

Will you help in this regards

Thanking you.

0 Kudos
Reply
2 Replies

2,528 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the below link, you will find LPCOpen for Keil v5

LPCOpen Software for LPC43XX|NXP 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,527 Views
sujayp
Contributor II

I have gone through the link but i think i didnt find the user manual  to program the LPC4370 series using Keil Version 5 and keil Ulink2.

The link would only  include the Lpcexpresso and jlink deugger

0 Kudos
Reply