LPC436x and LPC4370 datasheet typos in section 7.3.1?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC436x and LPC4370 datasheet typos in section 7.3.1?

1,688 Views
AndrewBradford
Contributor I

In the LPC436x and LPC4370 datasheets, in section 7.3.1 "ARM Cortex-M0 coprocessor" it says:

"The M0 coprocessor resides on the same AHB multi-layer matrix as the main Cortex-M0 core."

Shouldn't this instead say:

"The M0 coprocessor resides on the same AHB multi-layer matrix as the main Cortex-M4 core."

The M0 coprocessor *IS* the main Cortex-M0 core, the main processor is the Cortex-M4 core.  The "ARM Cortex-M0 subsystem" is the *other* M0 core and it is not on the main AHB matrix, it has its own bus connected to the main AHB matrix via a bridge over with the SGPIO.

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,559 Views
bernhardfink
NXP Employee
NXP Employee

May I correct this :smileycool:

The Cortex-M4 and the Cortex-M0APP are connected as masters on the same AHB multi-layer matrix, the M0SUB is behind a bridge. So as you stated correctly:

"The Cortex-M0APP coprocessor resides on the same AHB multi-layer matrix as the main Cortex-M4F core."

This applies to all LPC4300 family members, only the LPC4367 and the LPC4370 include the additional M0SUB as well.

Regards,

Bernhard.

1,559 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Andrew Bradford,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
The LPC43xx/LPC43Sxx is a multi-core microcontroller implementing an ARM Cortex-M4
and one or two ARM Cortex-M0 cores, the M0 co-processor resides on the same AHB multi-layer matrix as the main Cortex-M0 core, and the other ARM Cortex-M0 core (M0SUB) as the Cortex-M0 subsystem.
So I don't think it's a typo.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply