LPC4357JBD208E vs LPC4357JBD208K

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4357JBD208E vs LPC4357JBD208K

ソリューションへジャンプ
3,457件の閲覧回数
amirnat
Contributor I

Hi, what is the difference between LPC4357JBD208E and LPC4357JBD208K ?

I searched in some distributors like Mouser and Digikey, they suggest to buy LPC4357JBD208K instead of LPC4357JBD208E, why? Is there any failure  or other issue? 

I have created a C project for LPC4357JBD208E, can I run it on LPC4357JBD208K ? 

Are LPC4357JBD208E and LPC4357JBD208K pin compatible? can I solder LPC4357JBD208K instead of LPC4357JBD208E?

thank you in advance.

 

0 件の賞賛
返信
1 解決策
3,436件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Amir,

The answer is Yes, the silicon are the same for the LPC4357JBD208E and LPC4357JBD208K, you can  replace any of them with each other without any software and/or hardware consideration.

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,447件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to the link:

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

 

The LPC4357JBD208E package contains 36 PCS, but the LPC4357JBD208K package contains 180 PCS.

LPC4357JBD208E

Active

 

LPC4357JBD208K

Active

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信
3,442件の閲覧回数
amirnat
Contributor I

Thank you dear  xiangjun_rong,

Can I replace any of them with each other without any software and/or hardware considerations?

0 件の賞賛
返信
3,437件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Amir,

The answer is Yes, the silicon are the same for the LPC4357JBD208E and LPC4357JBD208K, you can  replace any of them with each other without any software and/or hardware consideration.

BR

XiangJun Rong

0 件の賞賛
返信
3,433件の閲覧回数
amirnat
Contributor I

Thank you very much.

0 件の賞賛
返信