LPC4357

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4357

1,607 Views
sudheerkumardor
Contributor I

Hi every one,

I used LPC4357 BGA package in my project. I want to communicate with the other controller using Ethernet communication. For that i want Ethernet Drivers of LPC4357 controller. Can any one give the link to download the drivers of Ethernet. 

Thanks to NXP.

Labels (1)
0 Kudos
Reply
1 Reply

1,439 Views
soledad
NXP Employee
NXP Employee

Hi,

You can check the LWIP packet. ethernet | www.LPCware.com 

However, The standalone LWIP port has been replaced with the LPCOpen version of LWIP. The LPCOpen version supports more examples.

You can download the LPCOpen from LPCOpen Software for LPC43XX|NXP 

In addition you can check the below link:

MDK5 - NXP LPC4357 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply