LPC4357: modification of images for DFUsec

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4357: modification of images for DFUsec

1,386 Views
quex
Contributor I

I'd like to download images to my LPC4357 using  DFUSec (Two projects: M4 & M0App).

From the forum I understood, that I need a tool to modify the binaries.

Unfortunately the link does not work any more:

http://lpcware.com/content/nxpfile/lpc18xx-43xx-image-manager

Where could I get the image manager from?

Thanks

Labels (3)
0 Kudos
Reply
3 Replies

1,151 Views
quex
Contributor I

Thank you, I'll try that.

0 Kudos
Reply

1,151 Views
lpcxpresso_supp
NXP Employee
NXP Employee

DFUSec was superseded by LPCScrypt sometime ago  : http://www.nxp.com/lpcscrypt

Installing LPCScrypt will also provide the "image manager tool", though you don't need this for programming images into internal flash.

Regards,

LPCXpresso Support

0 Kudos
Reply

1,151 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the below link and let me know if this helps.

USB DFU Firmware Upload for LPC1850 LPC4350 LPC1800 LPC4300 LPC18xx LPC43xx 


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply