LPC4357 bootloader dump

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4357 bootloader dump

3,818 Views
pieroquark87
Contributor I

Hi there,

I would like to know if is it possible to dump the bootloader flashed on the internal ROM of the LPC4357 tracing back to the corresponding bin file.

Many thanks in advance.

Giovanni

Labels (1)
0 Kudos
Reply
5 Replies

3,814 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

No, you can't put your own bootloader in the ROM, the ROM already has the definite bootloader and can't be erased before out of the factory.

If you want to use the customized bootloader, you should put it in front of the flash.

Best regards,
Pavel

0 Kudos
Reply

3,809 Views
pieroquark87
Contributor I

Hi, yes, sorry, I said that badly. I meant I've loaded onto the flash A memory a custom bootloader using the Ulink Pro. After that if, for example, I give the board to you, is there a way you can trace back to the corresponding bin file of the custom bootloader I've loaded?

0 Kudos
Reply

3,803 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

Yes, sure, but are you interested in locking the MCU? 

Best regards,
Pavel

0 Kudos
Reply

3,796 Views
pieroquark87
Contributor I

Hi, thanks for your reply. How do you make to trace back to the custom bootloader bin?

 

0 Kudos
Reply

3,748 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

What do you mean with |trace back|? Is that for TRACE or Reverse engineering?

I meant I've loaded onto the flash A memory a custom bootloader using the Ulink Pro. After that if, for example, I give the board to you, is there a way you can trace back to the corresponding bin file of the custom bootloader I've loaded?

I think we have different understanding could you please elaborate further?

If you want to use a secure bootloader I think this app note maybe could help you.
[Secure Bootloader implementation (nxp.com)] [Firmware Update Using Secondary Bootloader (nxp.com)]

Best regards,
Pavel

0 Kudos
Reply