LPC4357 VBAT current consumption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4357 VBAT current consumption

1,225 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by michele sponchiado on Thu Jul 16 00:45:48 MST 2015
Hi,
we're using an LPC4357, and we're checking the current consumption from VBAT with powered off chip.
We measured 70 microAmpères before applying the patch suggested in the LPC435x errata sheet (in the paragraph 4.1).
Then we applied the patch, so that RTC_ALARM and SAMPLE pins are now set to inactive, and we measure now about 8 microAmpères.
This is considerably better, but I was expecting something less, about 4 or 5 microAmpères.
Are there any other tricks to reduce VBAT current consumption or this is the minimum we can attain with powered down chip?
Thanks!
Labels (1)
0 Kudos
Reply
1 Reply

1,187 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Thu Jul 16 22:32:31 MST 2015
Hi Michele,

On the LPC43xx Rev'-' version , this is expected. On the Rev 'A' devices this errata has been fixed.

Thanks
NXP Technical Support
0 Kudos
Reply