LPC4357 USB ROM stack

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4357 USB ROM stack

1,991 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dziobal89 on Fri Mar 01 04:17:38 MST 2013
When I'm using the npxusblib with the USE_USB_ROM_STACK USB_Init() isn't configuring USB controller (interrupts are not turned on in the controller). Looks like the USBD_API->hw->Init in UsbdRom_Init() doesn't work properly but it returns LPC_OK. USB ROM Stack isn't working even if I configure the USB Controller by hand. I'm using the LPC4357 OEM Board produced by Embedded Artists. Have anybody had the same problem? Sorry for my poor english.
Labels (1)
0 Kudos
Reply
3 Replies

1,936 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dziobal89 on Mon Mar 04 11:22:37 MST 2013
You are right! I haven't noticed it. It is here http://www.nxp.com/documents/user_manual/UM10503.pdf on the page 644. I must not ignore introduction parts of manuals. Thank your very much.
0 Kudos
Reply

1,936 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wellsk on Mon Mar 04 11:22:00 MST 2013
I've used it before for DFU class on a number of 18xx/43xx devices and haven't had any problems with it.
Maybe the DFU USB (ROM) examples in LPCOpen may help?

http://docs.lpcware.com/lpcopen/group___e_x_a_m_p_l_e_s___d_f_u_u_t_i_l__18_x_x43_x_x.html
0 Kudos
Reply

1,936 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mark03 on Mon Mar 04 11:04:11 MST 2013
I remember reading the documentation and not being 100% clear on whether the USB ROM stack was even preset in the flash parts.  If you read it literally it seems to imply that this is only present on the LPC4330 and LPC4350.  Maybe someone else can confirm/deny?  Because I'm curious too.
0 Kudos
Reply