LPC4357 USB CDC driver to interface LTE module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4357 USB CDC driver to interface LTE module

2,444 Views
TEMCEFF
Contributor IV

Hi,

We would like to interface a LTE module with the High Speed USB interface of LPC 4357 . i.e, LPC4357 would be the host and module will be the device. So kindly provide us the LPC4357 Communication Device class driver as well as any application notes to interface the LTE modules

Labels (2)
0 Kudos
Reply
3 Replies

1,921 Views
TEMCEFF
Contributor IV

Hi Carlos,

Thanks for the reply,

We have gone through the Example and it is useful for the initial development. We would like to use Integrated USB DMA for our application. Could you help us regarding the configuration of USB DMA for the Host mode. 

0 Kudos
Reply

1,921 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Anusha,

Unfortunately we don't have an example of this configuration.

Best Regards!
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply

1,921 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Anusha,

Take a look to the following thread:

https://community.nxp.com/message/749278 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer