LPC4357 TFT Display 4Bit each colour without external RAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4357 TFT Display 4Bit each colour without external RAM

2,959 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Georg on Mon Dec 01 01:04:57 MST 2014
Hi,

i use a LPC4357 with a small TFT (320x240) display. This display is connected over 16Bit HW-Interface
and work fine. But for this funktion i need a external ram for the framebuffer.

I need a solution to run this TFT without external RAM. I would use it with 4bit each colour.
But i don't understand how to initialise the colourpalette for this mode.

Can someone give me some examples or help to initialise the tft.
Cursor works fine in 4Bit mode.

thx.

Georg.
标签 (1)
0 项奖励
回复
4 回复数

2,829 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Georg on Mon Dec 15 03:56:18 MST 2014
Hi,

i need only to know how to config the LCD-Controller from LPC and the
Color Palette registers to run my display with 4 Bit and so save memory.
Ich will only use internal memory of LPC µC.

Thx.

Regards,

Georg.
0 项奖励
回复

2,829 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Georg on Tue Dec 02 03:47:15 MST 2014
Hi,

i Use a Onation OT035AQDDDT display with a HX8238 controller onbaord.
I drive this display wit the 16-bit HW-Interface and i use the lcd-controller from lpc.
For framebuffer i use the external RAM. But i need a solution without ext. RAM.
4Bit colourdepth is enough for my application.

I can configure the lpc lcd-controller to work with 4Bit. But i can not display some
colours. Only the cursor for my touch works and is displayed on lcd.

Thx.

Regard,
Georg.
0 项奖励
回复

2,821 次查看
magdiel3
Contributor I

How did you manage to do so?

0 项奖励
回复

2,829 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Martin84 on Tue Dec 02 02:53:08 MST 2014
Which TFT is it? May be a Sainsmart-TFT? I think your TFT has an internal LCD Controller (i.e. SSD1289) which you drive with the 16-bit HW-Interface. These LCD Controllers have a internal RAM as Framebuffer which you can use. But I don't know if you can use this TFT-Framebuffer with the LPC LCD-Controller.

If there's such a LCD-Controller like the SSD1289 you can drive the TFT with the LPC EMC or with GPIO-Lines.

Regards,

Martin
0 项奖励
回复