LPC4357 SDRAM connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4357 SDRAM connection

1,381件の閲覧回数
anagoncalves
Contributor I

Hi,

Must I use CLK1 to connect a 16x SDRAM to KPC4357 to reach 104MHz? If I use CLK0 instead of CLK1 there is a chance to reach the maximum speed?

Thanks,

0 件の賞賛
返信
1 返信

1,274件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Ana,

When using only one external chip, use the CLK1 or CLK3 pin to drive the SDRAM clock for best performance. CLK0 and CLK2 pins are used for SDRAM read capture feedback clocks and must not be used for any other function.

There is an errata at below link. Please check it if you are planning to use high SDRAM frequencies:

http://www.nxp.com/documents/errata_sheet/ES_LPC435X_3X_2X_1X_FLASH.pdf 

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信