LPC4357 LPCScrypt USB0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4357 LPCScrypt USB0

ソリューションへジャンプ
2,075件の閲覧回数
vonp
Contributor II

Hi,

I am trying to use LPCScrypt and windows to program my application onto a custom board using the LPC4357 mcu. After setting P2_8,P2_9, P1_2 and P1_1 to select USB0 as well as setting  P2_7 LOW on reset I cannot get the virtual port to emulate on windows.

 device_manager.JPG

lpcscrypt.JPG

I have installed LPCScrypt_2.1.1_15.exe as well as lpc_driver_installer.exe. Am I missing something else?

ラベル(3)
0 件の賞賛
返信
1 解決策
2,003件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Heath Pritchett,

1) First please confirm config the boot pins as below:

pastedImage_3.png

2) We need to download LPCScrypt firmware to the target MCU:

pastedImage_4.png

Regards,

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,004件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Heath Pritchett,

1) First please confirm config the boot pins as below:

pastedImage_3.png

2) We need to download LPCScrypt firmware to the target MCU:

pastedImage_4.png

Regards,

Alice

0 件の賞賛
返信