LPC4357 I2S

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4357 I2S

1,492 次查看
athulpavithran
Contributor I

Hi,

I am currently working with i2s peripheral of lpc4357. The ultimate aim is to ingrate audio codec SGTL5000 with lpc4357. I am little confused over i2s 4-line, That is the SGTL5000 has got four i2s pins 1)DOUT  2)DIN  3)SCK 4)WS  where as  lpc4357 found to be eight pins  1)RX_SDA  2)TX_SDA  3)RX_SCK  4)TX_SCK  5) RX_WS 6)TX_WS 7)RX_ MCLK 8)TX_MCLK. I am not understanding the purpose of RX_MCLK and TX_MCLK. How do i interface sgtl5000 4-line i2s with lpc4357 3-line i2s(separate for RX and TX) ?.I didn't find any relevant document to refer. Looking for replay.

Thank you.

标记 (1)
0 项奖励
回复
1 回复

1,316 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Athul Pavithran,

LPC435x I2S interface also can be set as 4-pin mode.

You can connect the pins coresponding the application.

More information, you can refer to LPC43xx UM section: 43.7.2 I2S operating modes
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复