LPC4357 - HID output and input report low throughout

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4357 - HID output and input report low throughout

1,834 Views
ssudhir
Contributor II

Hi,

We are using LPC4357 and using NXP USB ROM driver for HID communication. The output report we send from the host arrives via EP OUT rather than control out.  So, when a host sends output report, at the device side set_report function doesn’t get called instead  HID_Ep_Hdlr gets called. The throughput for set and get report (we send 64 bytes output report and get 64 bytes input report – our program  echoes) is around 500 milliseconds . When we send 100 output report and get 100 input reports it takes 55 seconds. Feature report size is 255 and sending 10 -  500 bytes feature report and getting 500 bytes response takes less than second. Feature reports are sent and received via control out and input. In both cases we echo back. We segment and desegment feature reports so that we can send 500 bytes at a time which is much more complicated. Do you have any idea why the throughput for EP OUT is so low? Is there any way to receive output report via control out so that set_report gets called for output report?

Thanks

0 Kudos
Reply
2 Replies

1,759 Views
ssudhir
Contributor II

Output report handler arrives only on EP in HID and we are using ROM driver. There is patch up may be that is causing the delay. We need to improve our throughput and we can get output report via control. We have bit of time crunch. So please let us know.

0 Kudos
Reply

1,759 Views
soledad
NXP Employee
NXP Employee

Hi, 

Please check the following link and let me know if this helps, 

https://ravikiranb.com/tutorials/generic-comm-usb-hid/

Have a nice day 

Regards 

Soledad

0 Kudos
Reply