LPC4357-EVB write and read file to SD eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4357-EVB write and read file to SD eMMC

1,419 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by marcosbontempo on Fri May 06 06:43:10 MST 2016

Hello,

I'm using a LPC4357-EVB kit, which has a SD eMMC interface. I found this example that reads a WAV file from the SD and plays it:

https://www.element14.com/community/docs/DOC-62637

However, I also need to write a file into the SD.
Does anybody have a simple example that manipulates files in a SD card, using the LPC4357?

Any tip wil be very helpful,
Thanks.
Labels (1)
0 Kudos
Reply
2 Replies

1,257 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

1,257 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxpecosystem on Fri May 06 14:07:12 MST 2016
There is a full size SD card on the Hitex LPC4350 eval board, and on the LPC General Purpose Shield (which can be used with an LPCXpresso4337/4367 board.) LPCOpen packages for these boards include examples for read/write to a memory card over the SD eMMC interface. Hopefully these can help you out.
0 Kudos
Reply