LPC4357 C_CAN.1 Errata

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4357 C_CAN.1 Errata

2,018 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Thiapalm on Thu Mar 31 12:22:09 MST 2016
Hello,

We have an application that uses ADC, MCPWM and CAN.

We have been experiencing CAN problems and after some research, we have found the Errata sheet LPC435x/3x/2x/1x flash-based devices mentioning  BUS problems between CAN and the mentioned devices.

However, on the LPC43xx Datasheet from 15 of March 2016 (v5.3), it is said that the problem is solved since version v3 from 2014/08/19.

" Removed restriction on C_CAN bus usage. See CAN.1 errata in Ref. 2."

Is it really solved?

If so, how can I identify the "fixed" Chips?

Thx
Labels (1)
0 Kudos
Reply
5 Replies

1,947 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

1,947 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Thiapalm on Mon Apr 04 04:07:21 MST 2016
Thanks,

I will follow that thread....
0 Kudos
Reply

1,947 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mysepp on Sat Apr 02 05:32:56 MST 2016
See my thread here (started some days ago):
https://www.lpcware.com/content/forum/auto-detect-code-lpc4357-rev-or-rev
0 Kudos
Reply

1,947 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Thiapalm on Fri Apr 01 05:04:02 MST 2016
Hi,

That's true, I have not read that chapter on the errata.

Is there a way to identify the chip revision by reading the chip memmory using IAP for example?

Thanks for the help.
0 Kudos
Reply

1,947 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mysepp on Thu Mar 31 13:14:54 MST 2016
Please read again the errata sheet.
Chapter 1 explains how to identify the chip by interpreting the numbers printed on the chip.
0 Kudos
Reply