LPC4353JBD208 question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4353JBD208 question

Jump to solution
3,172 Views
uzunov16
Contributor I

Hello, I'm new in fixing electronics. I'm trying to fix my ploter PCB and i cheked with multimeter the capacitors. Every capacitor around the LPC4353JBD208 seems to be shorted. Does that means the MCU is shorted and i need to replace it?

Thank you!

0 Kudos
Reply
1 Solution
3,132 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Okay, I suppose the MCU has broken down, you need a new one.

BR

XiangJun Rong

View solution in original post

0 Kudos
Reply
6 Replies
3,146 Views
uzunov16
Contributor I

I removed the MCU and now the capacitors are not shorted. That means i need new MCU?

0 Kudos
Reply
3,073 Views
uzunov16
Contributor I

Do i need a software to program the MCU after the replacement?

0 Kudos
Reply
3,050 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The LPC4353 has on-chip flash, I suppose that you have to program your application code to the flash.

If you have the source code project, you can use keil, IAR or MCUXPresso tools to download the code.

If you has the *.bin or S_record file, you can use FlashMagic tools to download the code in ISP mode.

https://www.flashmagictool.com/download.html&d=flashmagic

 

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply
3,133 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Okay, I suppose the MCU has broken down, you need a new one.

BR

XiangJun Rong

0 Kudos
Reply
3,155 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that the VDD and GND pins are shorted either on board or inside silicon. Pls remove the LPC4353 from board and check if the shorting happens or not.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply
3,153 Views
uzunov16
Contributor I

Thank you! I'll try it.

0 Kudos
Reply