LPC4350FET256 Peak Reflow Temperature

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4350FET256 Peak Reflow Temperature

735件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gregd on Wed Sep 23 12:56:10 MST 2015
Can anyone tell me the peak reflow temperature for the LPC4350FET256.  We are having some problems with the BGA consistently reflowing.  We are planning to adjust the dwell time and/or temperature to hopefully correct the problem and want to make sure we are not exceeding any temperature limits.  I do not see the limit in the spec sheet.

ラベル(1)
0 件の賞賛
返信
0 返答(返信)