LPC4350 Hitex eval board, LWIP TCPIP_ECHO() code , HARDFAULT()

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4350 Hitex eval board, LWIP TCPIP_ECHO() code , HARDFAULT()

1,505 次查看
soorajkumar
Contributor I


Hi,

I am trying to run TCPECHO() code on Hitex 4350 eval board ,provided by LPCOPEN which uses LWIP stack. When i am downloading the code using my JLINK debugger and start the execution, it is found that the code doesnt respond, so when a break is executed it is seen that the code has entered a HARDFAULT_HANDLER().

I have checked the jumper settings required for ethernet to be enabled and they are proper. Since it is a reference example, I expected it to work fine.

I am using IAR 6.5 IDE and lpcopen V1.03 code. is there any specific setting that needs to be done in the code or on the hitex eval board to make the ethernet work? Basically what I expect is that I should be able to get a ping.

please help as soon as possible.

Thanks and regards,

Sooraj.

标签 (3)
标记 (1)
0 项奖励
回复
1 回复

1,254 次查看
soledad
NXP Employee
NXP Employee

Hi,

Could you please try using the default jumper settings?

Please try using the workflow steps that you can find in the next link:

http://www.freertos.org/FreeRTOS-Plus/BSP_Solutions/NXP/LPCOpen_lwIP_FreeRTOS.htm

Please let me know if this helps!

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复