LPC4337: measuring 2 different analog signals at ADC0_ch1 and ACD1_ch1?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4337: measuring 2 different analog signals at ADC0_ch1 and ACD1_ch1?

1,128 次查看
andreasklockner
Contributor II

Hello,

we are using the LPC4337.

We're investigating whether it's possible to measure TWO DIFFERENT analog signals (let's call it signal A and B) with ADC0 channel 1 and ADC1 channel 1?

- we have connected signal A to the dedicated analog Pin "ADC0_1/ADC1_1"

- we have connected signal B to PC_0 (which shall be routed internally to ADC1)

At the moment it seems, that analog signal A and signal B are "some kind of connected" within the LPC4337?

UserManual, Chapter 17 says: "This means that for the parts with shared input channels, input ADC0_n is connected to
channel n on ADC0 and ADC1 and input ADC1_n is connected to channel n on ADC0 and
ADC1, See Table 197 and Table 199".

Is that true? Are channel 1 of ADC0 and ADC1 really connected internally?

If I understand this correctly, it would mean that ADC0 channel 1 and ADC1 channel1 could not be used to measure 2 different analog signal independently?

Or is there a way to configure the LPC4337 so that the two analog signals (Pin "ADC0_1/ADC1_1" and Pin "PC_0)  do not electrically influence each other?

标签 (2)
标记 (2)
0 项奖励
回复
1 回复

1,091 次查看
andreasklockner
Contributor II

Ok, I think I found the answer to my question:

It is NOT possible to measure 2 different analog signals at ADC0_ch1 and ACD1_ch1, because they are tied together internally in the LPC4337.

See post:

about ADC 

0 项奖励
回复