LPC4337 UART0 IS HANGING WHEN CONNECTING WITH FTDI TTL232R

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4337 UART0 IS HANGING WHEN CONNECTING WITH FTDI TTL232R

1,707件の閲覧回数
aravindmuttinen
Contributor I

We are using LPC4337 controller in one of our project. UART0 i am using for configuration over by connectiong FTDI TTL232R to PC. Sometimes it is working sometimes the controller is hanging. What is the problem?.

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,571件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi aravind muttineni,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.

The UART hanging issue is very typical and it can be caused by hardware or software design.

So I was wondering if you can describe the flow which triggers the issue happen definitely, then it can help me to figure out the root cause of the issue.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信