LPC4333JET256使用时温度过高

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4333JET256使用时温度过高

963 Views
maggiepan
Contributor I

LPC4333JET256使用时温度过高

0 Kudos
Reply
5 Replies

836 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

能否提供详细的LPC4333JET256功耗信息?

能否提供使用到LPC4333JET256内部哪些模块?


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

836 Views
maggiepan
Contributor I

你好,

具体情况如下:

1.目前的测试所有外设都已经去掉

2.SDRAM, FRAM, SP706

3.Schematic在此链接,请下载查看

http://pan.baidu.com/s/1kVFUaft 

4.VDD 3.28V

5.电流55mA

6.已经检查过,未能发现什么问题

7.Cortext-M4 204MHz; Cortext-M0 204MHz

请提供关于这款芯片运行中各个频率时的温度参数,我们以用来参考目前温度是否正常,谢谢。

Maggie pan

www.sun-glow.com

xmrita@163.com

0 Kudos
Reply

836 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Maggie,

不好意思,我们没有芯片运行时各个频率的温度参数,只有功耗跟主频和温度的变化曲线:

pastedImage_1.png

有没有具体的温度数据,环境温度多少度?芯片表面温度多少度?


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

836 Views
maggiepan
Contributor I

你好,

请问flash bank A/B 加速器配置的FLASHTIM的位值寄存器地址是多少,如何操作,因为这个芯片寄存器太多了,  没有找到。

另,请问贵司能否使用电话等联系方式,以及派工程师上门解决技术问题,谢谢。

Maggie pan

www.sun-glow.com

xmrita@163.com

0 Kudos
Reply

836 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

你好, Maggie

请参考下面的信息配置FLASH BANK A/B加速配置寄存器:

Flash Accelerator Configuration for flash bank A register (FLASHCFGA, address 0x4004 3120);

Flash Accelerator Configuration for flash bank B register (FLASHCFGB, address 0x4004 3124).

Following reset, flash accelerator functions are enabled and flash access timing is set to a default value of 16 clocks.

If customer want to modify the [FLASHTIM] value of FLASHCFGA/B register, please refer below code:

LPC_CREG->FLASHCFGA = (0xF << 12) | (0x1 << 31);

LPC_CREG->FLASHCFGB = (0xF << 12) | (0x1 << 31);

我们提供在线支持。如果想要现场支持,请联系你当地NXP代理商,他们会提供上门支持的。

你当地的NXP代理商联系方式可以通过这里找到。

商祺。
Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply