LPC4330FET180 external flash support.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4330FET180 external flash support.

1,511 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kumarbhimesh on Thu Dec 18 22:56:26 MST 2014
Hi,

We have custom LPC4330FET180 based custom board. In this We used N25Q064A13ESE40E external flash.

Does this LPC4330 supports the above mentioned NOR flash for ROM booting ?

Does ROM boot having the support for N25Q064A13ESE40E  flash ?

What is the ROM version is used in this LPC4330 and how i can check it ?




Regards,
Bhimesh.

标签 (1)
0 项奖励
回复
2 回复数

1,485 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri Dec 19 12:08:25 MST 2014
Hi Bhimesh,
LPC4330 will boot from Micron N25Q064A when both devices are powered(cold boot).There will be problem when LPC is reset and Micron QSPI flash is not reset and is in XIP mode.
If you have planned reset you can make N25Q064A to exit out of XIP mode and reset LPC4330.
0 项奖励
回复

1,485 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kumarbhimesh on Fri Dec 19 03:27:53 MST 2014
Hi,

Please reply me.

Regards,
Bhimesh.
0 项奖励
回复