LPC4330 part ID

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4330 part ID

1,708件の閲覧回数
cyc583723081
Contributor I

hi,

I read this in the user manual of lpc43xx ,"IAP commands are only supported for parts with on-chip flash. "

lpc4330 has no flash on it, so how do lpc4330 read part identification number?

0 件の賞賛
返信
2 返答(返信)

1,590件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the below thread,

Device Serial Number 

I hope this helps,

Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,592件の閲覧回数
cyc583723081
Contributor I

hi,

Thank you very much for your letter.

I learned that a part id can be read from an otp memory bank0, but the otp Driver does not provide an API.Here's what the user manual says:  "For flashless parts only: The unique part ID can be read from OTP bank 0, words 0 to 3 at memory location 0x4004 5000."

How can I access this address?

0 件の賞賛
返信