LPC4330 ethernet- remote wake up frame filter.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4330 ethernet- remote wake up frame filter.

731 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Krishnakumar on Mon Sep 29 04:38:21 MST 2014
Hi folks,

In LPC4330 ethernet, It has a register called remote wake up frame filter(WAKEUPFMFILTER_REG) which is used for wake on lan configuration by wake up farme.

The WAKEUPFMFILTER has a field called "filter i CRC_16" which is 16 bits wide. In the document UM10503.pdf it's given that this "filter i crc_16" field contains CRC_16 value calculated for the pattern and the byte mask programmed to the wake-up filter register block.

But the byte mask is of 32 bits and how a field of 16 bits wide that is "filter i CRC_16" contains 16 bits CRC(CRC_16 for pattern) and the 32 bits byte mask. Let me know, if is there any logic behind that?


Thanks and regards,

Krishnakumar Kulkarni
Labels (1)
0 Kudos
Reply
0 Replies