LPC4330-Xplorer board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4330-Xplorer board

5,912 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jdurand on Wed Mar 28 12:26:12 MST 2012
Anyone have a schematics or other documentation for this new board?  Our company got a couple of them at Design West yesterday but they don't come with any documentation and the NGX Technologies site is useless (also says the board costs $2,500.00 which I think is a "small" error).

I need this to continue development since the Hitex LPC4350 board I have is version A2 and Code Red doesn't support it (too old).
标签 (1)
0 项奖励
回复
16 回复数

5,871 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drs on Mon Jun 11 16:54:17 MST 2012
You can boot up the board over USB using this tool: http://www.lpcware.com/content/project/dfu-downloadupload-lpcdfusec-tool

You will need to set the boot jumper block (J4) to boot up via USB. You will find the required settings in the UM.
0 项奖励
回复

5,873 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pdv on Mon Jun 11 13:26:08 MST 2012
Hi, I'm also an absolute beginner.

What documentation do you mean? The manual is available on the ngx website and also the examples. Is there anything else?
The little information included with the board still suggests to register to get the documentation, but that's probably outdated.

The manual only refers to testing with a PC but it works also fine with a mac: I've installed the VPC drivers from ftdi (see http://www.ftdichip.com/Drivers/VCP.htm) and used the goSerial terminal emulator (see http://www.furrysoft.de/?page=goserial).

[The VPC drivers are actually not needed. The drivers installed with openOCD work fine]

Next I'll check the olimex debugger and openOCD.

[The current (macport) version of openOCD 0.5.0 has no script for the lpc43xx target, but the source at the openOCD repository contains a basic script for the lpc4350.cfg which works with the Xplorer board and the olimex jtag debugger.]
0 项奖励
回复

5,871 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shaunak on Fri May 25 21:01:29 MST 2012
I just received my board. I am still waiting on the documentation, which I hope will clarify a few things and will contain enough information for me to get started.

Im an absolute beginner and am little confused if need additional hardware to program the board or if I should be able to do it over USB with a bootloader? It is not really clear on the website.
0 项奖励
回复

5,871 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ashwin_athani on Wed May 16 03:51:43 MST 2012
Please note that the dual-core debug support is currently, only support by KEIL uvision V4.5 and ulink/ME combination. LPCXpresso and LPC-link combination does not offer a out of box experience at the moment. However, we have provided the examples for the LPCXpresso on our product page. We will continue to add support for more IDEs and debuggers going ahead but we highly recommend KEIL uvision V4.5 and ulink/ME combination for now. Also the uvision V4.5 has integrated the external Flash Driver files (FLM) for the external Q-Flash, therefore debugging and programming onto Q-flash is easier as compared to V4.23 (where these files had to be added externally).

We are updating the examples to V4.5 and will be releasing the same on 18th of this month.

-Ashwin

0 项奖励
回复

5,872 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by steph_tsf on Tue May 15 00:45:56 MST 2012
I've just ordered :
2 x LPC4330 Xplorer boards from NGX
2 x LPC1227 LPCXpresso LPC-Link from Embedded Artists
Let's cross the fingers ...
0 项奖励
回复

5,871 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ashwin_athani on Fri Apr 06 01:09:06 MST 2012
@Jerry,
For the LPC4330 the Code Red defaults to JTAG interface for debugging. Try switching to SWD.
See here http://support.code-red-tech.com/CodeRedWiki/ConnectingToJtag.
We are working on the LPCXpresso examples and the first release is planned next week.

0 项奖励
回复

5,871 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ashwin_athani on Fri Apr 06 01:03:44 MST 2012
Please plug in a SD card formatted with FAT filesystem and the message should go. I must admit that the message is a little misleading. It should be stating that the "SD card is missing", we are working on a new release of the sample programs for the Xplorer.
0 项奖励
回复

5,871 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jdurand on Wed Apr 04 12:13:11 MST 2012
Since I switched to Code Red I've had some problems loading code and debugging on the board (communications errors).  Code Red received one of these boards the day after I got mine and were going to check into the problems. I haven't heard back so I don't know where they're at with it.
0 项奖励
回复

5,871 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by imikec on Wed Apr 04 11:28:26 MST 2012
I am having a problem trying to excercise this board. When I connect USB to usb1 I can see message SDIO failed, repeated all the time. What can be the problem?
0 项奖励
回复

5,871 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dima2611 on Fri Mar 30 18:30:22 MST 2012
2500 Rupee, not USD. So just around 40 USD
0 项奖励
回复

5,871 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jdurand on Thu Mar 29 10:17:16 MST 2012
I received a reply to my product registration today and am downloading the documentation Zip now (41.9MB in size, sounds like lots of stuff in there).
0 项奖励
回复

5,871 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gdcooper on Thu Mar 29 10:09:42 MST 2012
NGX has updated their site with the NGX Xplorer board user's manual. Registered users get the schematics and code examples. $2,500 per board? What a great value you got at Design West!

Here's the NGX link:
http://shop.ngxtechnologies.com/product_info.php?cPath=21_37&products_id=104
0 项奖励
回复

5,871 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drs on Wed Mar 28 19:57:06 MST 2012
Look here: nxpUSBlib v0.93\libraries\BSP\Schematics\HITEX_Final_LPC1850EVA-A3.pdf
0 项奖励
回复

5,871 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jdurand on Wed Mar 28 16:54:15 MST 2012
I'm looking through nxpUSBlib v0.93.zip but don't see a PDF file in there anywhere.  Is it someplace else?

Also, how do you tell the version on the LPC4330-Xplorer board?  I can't find a version on it anywhere unless it's under the serial number or CE stickers.

0 项奖励
回复

5,871 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jdurand on Wed Mar 28 16:44:50 MST 2012
Thanks, downloading now.
0 项奖励
回复

5,871 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drs on Wed Mar 28 16:25:16 MST 2012
The latest release of nxpUSBlib has a copy of this schematic, although the filename contains "A3" even though it is for the A4 board.

http://www.lpcware.com/content/project/nxpusblib
0 项奖励
回复