LPC4330-Xplorer Development Board receiving the ADC values

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4330-Xplorer Development Board receiving the ADC values

1,501 Views
eugenr
Contributor I

I'm trying to retrieve the ADC value, and I am using the Chip_ADC_ReadValue() method. But he only enters the Handler method once and not always when the input at the ADC pin changes. I am still not totally aware of what I am doing since I am new in programming micro controllers. I hope somebody can help me.

This is my ADC_Init():

static void ADCInit(){
     uint32_t _bitRate = 400000;
     ADC_RESOLUTION_T _bitAccuracy = ADC_10BITS;

     Chip_ADC_Init(LPC_ADC0, &ADCSetup); //Initialize the ADC Pin
     Chip_ADC_EnableChannel(LPC_ADC0, ADC_CH1, ENABLE);
     Chip_ADC_Int_SetChannelCmd(LPC_ADC0, ADC_CH1, ENABLE);//Enable Channel 1 of the ADC0 Pin for Interrupt
     Chip_ADC_SetStartMode(LPC_ADC0, ADC_START_NOW, ADC_TRIGGERMODE_RISING);//Set it to trigger on the rising event, Set Mode on starting the conversion now

     Chip_ADC_SetSampleRate(LPC_ADC0, &ADCSetup, _bitRate);//Set the sample rate to 400kHz
     Chip_ADC_SetResolution(LPC_ADC0, &ADCSetup, _bitAccuracy);//Set the accuracy to 10 Bits if one is using more channels the accuracy has to be dropped


     /*Enable Interrupt*/
     NVIC_SetPriority( ADC0_IRQn, (configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY));
     NVIC_EnableIRQ( ADC0_IRQn );

}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

And this is my Interrupt Handler:

void ADC0_IRQHandler(void)
{
     uint16_t dataADC;
     /* Interrupt mode: Call the stream interrupt handler */
     Chip_ADC_Int_SetChannelCmd(LPC_ADC0, ADC_CH1, ENABLE);
     Chip_ADC_ReadValue(LPC_ADC0, ADC_CH1, &dataADC);
     SetADCValue(dataADC);
     storeItemInfftBuffer(dataADC);
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Thanks in advance 

0 Kudos
Reply
1 Reply

1,358 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hello eugenr,

   You can refer to the lpcopen code for mcb 4357, there has the adc code.

   http://www.nxp.com/downloads/en/software/lpcopen_3_01_keil_iar_mcb_4357.zip 

   It seems you didn't enable the burst mode, if yes, the ADC conversions are software controlled, you need to call :

Chip_ADC_SetStartMode(_LPC_ADC_ID, ADC_START_NOW, ADC_TRIGGERMODE_RISING);

After the ADC convert done, then trigger the next adc conversion.

 /* Interrupt routine for ADC example */
static void App_Interrupt_Test(void)
{
    /* Enable ADC Interrupt */
    NVIC_EnableIRQ(_LPC_ADC_IRQ);
    Chip_ADC_Int_SetChannelCmd(_LPC_ADC_ID, _ADC_CHANNLE, ENABLE);
    /* Enable burst mode if any, the AD converter does repeated conversions
       at the rate selected by the CLKS field in burst mode automatically */
    if (Burst_Mode_Flag) {
        Chip_ADC_SetBurstCmd(_LPC_ADC_ID, ENABLE);
    }
    Interrupt_Continue_Flag = 1;
    ADC_Interrupt_Done_Flag = 1;
    while (Interrupt_Continue_Flag) {
        if (!Burst_Mode_Flag && ADC_Interrupt_Done_Flag) {
            ADC_Interrupt_Done_Flag = 0;
            Chip_ADC_SetStartMode(_LPC_ADC_ID, ADC_START_NOW, ADC_TRIGGERMODE_RISING);
        }
    }
    /* Disable burst mode if any */
    if (Burst_Mode_Flag) {
        Chip_ADC_SetBurstCmd(_LPC_ADC_ID, DISABLE);
    }
    /* Disable ADC interrupt */
    NVIC_DisableIRQ(_LPC_ADC_IRQ);
}

More details, please refer to the lpcopen code, or refer to my attached adc.c file.

If you still have question, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply