LPC4330 - USB Audio Device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4330 - USB Audio Device

890件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarekM on Tue Sep 29 08:17:44 MST 2015
Hi

I'm struggling to get the LPC4330 working as a USB Audio device, I tried the USB ROM library without any luck and now I'm looking at the LPCUSBLib but it seem to be obsolete??? I was hoping that someone could maybe tell me if the USB Audio Device is even doable on the LPC4330 device and if it is which way is the best way to go?

Thanks
Marek
ラベル(1)
0 件の賞賛
返信
0 返答(返信)