LPC4330 PLL1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4330 PLL1

1,370件の閲覧回数
tomsaluzzo
Contributor III

I’m having quite a bit of trouble changing the PLL1 clock frequency. Refer to the PLL1 Control Register on page 185 of the User Manual. Bit 11 is the “AUTOBLOCK” bit. I can’t find a description of this bit in the User Manual. What should this bit equal when I’m trying to change the BASE_M4_CLK frequency (see page 166 of the User Manual)?

ラベル(1)
0 件の賞賛
返信
1 返信

1,249件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tom,

The AUTOBLOCK flag prevents glitches of the output clock when switching from one input clock to another. Glitches may otherwise occur depending on the phase relation of the old and new clock. It is recommended to always use autoblocking.

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信