LPC4330 Custom Bootloader Request

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4330 Custom Bootloader Request

1,104件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fweller on Thu Mar 10 09:49:01 MST 2016
Our goal is to develop a custom boot loader that will upgrade an internal SPIFI (QSPI) application image with a file loaded from a removable SD Card.

We are requesting example code for this bootloader.
We could also use a good description of how this should be implemented, especially how to set up a LPCXpresso linker environment to build the main application that the bootloader would jump to when it is ready to execute from the SPIFI (SPI) application image.


ラベル(1)
0 件の賞賛
返信
1 返信

1,043件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信