LPC4320 can't DFU boot from USB0 ,help me

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4320 can't DFU boot from USB0 ,help me

1,147 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by g_turing on Tue May 13 10:21:44 MST 2014


hello,i'm using lpc4320FBD144 try to boot from USB0,can't enumeration,D+ D- voltage is zero. USB0_RREF voltage is 1.2v. P1_1 voltage is vcc ,3.3v. my soild temperature is 280 centi degree. where is wrong,somebody can tell me,thanks a lot!
[img=1861x1237]http://v2.freep.cn/3tb_140514011334jswo512293.jpg[/img]
Labels (1)
0 Kudos
Reply
1 Reply

1,115 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Wed May 14 16:00:13 MST 2014
Hi ,

The boot mode is determined by the states of the boot pins P2_9, P2_8, P1_2, and P1_1.
Please make sure the boot pins are in the following states to boot from USB0:

P2_9 - LOW
P2_8 - HIGH
P1_2 - LOW
P1_1 - HIGH

Refer to the following Application note for boot pin configuration to boot from various sources.

http://www.nxp.com/documents/application_note/AN11239.pdf

Thanks,
NXP Technical Support
0 Kudos
Reply