LPC411X: USB ROM Hard Faults with Composite Device with 3 CDCs VCOMs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC411X: USB ROM Hard Faults with Composite Device with 3 CDCs VCOMs

1,336件の閲覧回数
dean_sands
Contributor II

I'm trying to create a composite USB device with 3 CDC VCOMs. The code is hard-faulting when the USB IRQ Handler goes to the ISR. Everything looks good when bringing up the USB configuration with the USB ROM.

/******************************************/
/* Function Name: usb_cdc_connect         */
/* Return Type: ErrorCode_t               */
/* gets the parameters, creates the       */
/* handles, registers the endpoints IRQs, */
/* and connects to the USB                */
/******************************************/
ErrorCode_t usb_cdc_connect() {
    USBD_CDC_INIT_PARAM_T cdcParameters[3];
    ErrorCode_t ret = LPC_OK;
    uint32_t endpointIndex;
    uint32_t usb_block;
    uint8_t *ptr;
    char result;

    //Set Params
    memset((void *) &cdcParameters, 0, 2 * sizeof(USBD_CDC_INIT_PARAM_T));

    usb_block = usbParameters.mem_size / 4;
    ptr = usbDescriptors.high_speed_desc;
    cdcParameters[0].mem_base = usbParameters.mem_base;
    cdcParameters[0].mem_size = usb_block;
    cdcParameters[0].cif_intf_desc = ptr = (uint8_t *) findInterfaceDescriptor(ptr, CDC_COMMUNICATION_INTERFACE_CLASS);
    cdcParameters[0].dif_intf_desc = ptr = (uint8_t *) findInterfaceDescriptor(ptr, CDC_DATA_INTERFACE_CLASS);

    ret = USBD_API->cdc->init(g_hUsb, &cdcParameters[0], &g_hCDC[0]);
    PRINTF("Initializing first CDC...");
    result = (LPC_OK == ret);
    PRINTF(result ? "Successful\r\n" : "Failure\r\n");
    PRINTF("Return value: 0x%08X\r\n", ret);


    if (ret == LPC_OK) {
        endpointIndex = ((USB_CDC_IN_EP_0 & 0x0F) << 1) + 1;
        ret = USBD_API->core->RegisterEpHandler(g_hUsb, endpointIndex, bulkInHandler, &USB_CDC_Ctx[0]);
        if (ret == LPC_OK) {
            endpointIndex = ((USB_CDC_OUT_EP_0 & 0x0F) << 1);
            ret = USBD_API->core->RegisterEpHandler(g_hUsb, endpointIndex, bulkOutHandler, &USB_CDC_Ctx[0]);

        }
    }
    USB_CDC_Ctx[0].cdc = g_hCDC[0];
    USB_CDC_Ctx[0].in_endpoint = USB_CDC_IN_EP_0;
    USB_CDC_Ctx[0].out_endpoint = USB_CDC_OUT_EP_0;

    /* ############################################################################################## */

    cdcParameters[1].mem_base = usbParameters.mem_base + usb_block;
    cdcParameters[1].mem_size = usb_block;
    cdcParameters[1].cif_intf_desc = ptr = (uint8_t *) findInterfaceDescriptor(ptr, CDC_COMMUNICATION_INTERFACE_CLASS);
    cdcParameters[1].dif_intf_desc = ptr = (uint8_t *) findInterfaceDescriptor(ptr, CDC_DATA_INTERFACE_CLASS);

    ret = USBD_API->cdc->init(g_hUsb, &cdcParameters[1], &g_hCDC[1]);
    PRINTF("Initializing second CDC...");
    result = (LPC_OK == ret);
    PRINTF(result ? "Successful\r\n" : "Failure\r\n");
    PRINTF("Return value: 0x%08X\r\n", ret);


    if (ret == LPC_OK) {
        endpointIndex = ((USB_CDC_IN_EP_2 & 0x0F) << 1) + 1;
        ret = USBD_API->core->RegisterEpHandler(g_hUsb, endpointIndex, bulkInHandler, &USB_CDC_Ctx[1]);
        if (ret == LPC_OK) {
            endpointIndex = ((USB_CDC_OUT_EP_2 & 0x0F) << 1);
            ret = USBD_API->core->RegisterEpHandler(g_hUsb, endpointIndex, bulkOutHandler, &USB_CDC_Ctx[1]);

        }
    }
    USB_CDC_Ctx[1].cdc = g_hCDC[1];
    USB_CDC_Ctx[1].in_endpoint = USB_CDC_IN_EP_2;
    USB_CDC_Ctx[1].out_endpoint = USB_CDC_OUT_EP_2;

    /* ############################################################################################## */

    cdcParameters[2].mem_base = usbParameters.mem_base + (usb_block * 2);
    cdcParameters[2].mem_size = usb_block;
    cdcParameters[2].cif_intf_desc = ptr = (uint8_t *) findInterfaceDescriptor(ptr, CDC_COMMUNICATION_INTERFACE_CLASS);
    cdcParameters[2].dif_intf_desc = ptr = (uint8_t *) findInterfaceDescriptor(ptr, CDC_DATA_INTERFACE_CLASS);

    ret = USBD_API->cdc->init(g_hUsb, &cdcParameters[2], &g_hCDC[2]);
    PRINTF("Initializing third CDC...");
    result = (LPC_OK == ret);
    PRINTF(result ? "Successful\r\n" : "Failure\r\n");
    PRINTF("Return value: 0x%08X\r\n", ret);


    if (ret == LPC_OK) {
        endpointIndex = ((USB_CDC_IN_EP_3 & 0x0F) << 1) + 1;
        ret = USBD_API->core->RegisterEpHandler(g_hUsb, endpointIndex, bulkInHandler, &USB_CDC_Ctx[2]);
        if (ret == LPC_OK) {
            endpointIndex = ((USB_CDC_OUT_EP_3 & 0x0F) << 1);
            ret = USBD_API->core->RegisterEpHandler(g_hUsb, endpointIndex, bulkOutHandler, &USB_CDC_Ctx[2]);

        }
    }
    USB_CDC_Ctx[2].cdc = g_hCDC[2];
    USB_CDC_Ctx[2].in_endpoint = USB_CDC_IN_EP_3;
    USB_CDC_Ctx[2].out_endpoint = USB_CDC_OUT_EP_3;

    NVIC_SetPriority(USB0_IRQn, USB_DEVICE_INTERRUPT_PRIORITY);
    /*  enable USB interrrupts */
    NVIC_EnableIRQ(USB0_IRQn);
    /* now connect */
    USBD_API->hw->Connect(g_hUsb, 1);

    return ret;
}

 

const uint16_t config_desc_data_length = (           /* wTotalLength */
    (1 * USB_CONFIGURATION_DESC_SIZE) +      /* length of initial descriptor */
    (
        (1 * USB_INTERFACE_ASSOCIATION_DESC_SIZE) +  /* interface association descriptor */
        (1 * USB_INTERFACE_DESC_SIZE) +  /* communication control interface*/
        (5 + 5 + 4 + 5) +  /* CDC functions */
        (1 * USB_ENDPOINT_DESC_SIZE) +  /* interrupt endpoint */
        (1 * USB_INTERFACE_DESC_SIZE) +  /* communication interface */
        (2 * USB_ENDPOINT_DESC_SIZE) +  /* bulk endpoints */
        (0)
    ) * 3
);

/**
 * USB FSConfiguration Descriptor
 * All Descriptors (Configuration, Interface, Endpoint, Class, Vendor)
 */
ALIGNED(4)
uint8_t USB_FsConfigDescriptor[] = {
    /* Configuration 1 */
    USB_CONFIGURATION_DESC_SIZE,                /* bLength: 9 */
    USB_CONFIGURATION_DESCRIPTOR_TYPE,          /* bDescriptorType */
    WBVAL(config_desc_data_length),
    0x04,                                       /* bNumInterfaces */
    0x01,                                       /* bConfigurationValue: 0x01 is used to select this configuration */
    0x00,                                       /* iConfiguration: no string to describe this configuration */
    USB_CONFIG_BUS_POWERED /*|*/                /* bmAttributes */
    /*USB_CONFIG_REMOTE_WAKEUP*/,
    USB_CONFIG_POWER_MA(100),                   /* bMaxPower, device power consumption is 100 mA */

        /* ###################################################################################################### */
        /* First Interface Pair */
        /* Interface association descriptor IAD */
        USB_INTERFACE_ASSOCIATION_DESC_SIZE,        /* bLength: 8 */
        USB_INTERFACE_ASSOCIATION_DESCRIPTOR_TYPE,  /* bDescriptorType */
        USB_CDC_CIF_NUM_0,                          /* bInterfaceNumber: Number of Interface: 0 */ /* The first interface number associated with this function */
        0x02,                                       /* The number of contiguous interfaces associated with this function */
        CDC_COMMUNICATION_INTERFACE_CLASS,          /* bInterfaceClass: Communication Interface Class */
        CDC_ABSTRACT_CONTROL_MODEL,                 /* bInterfaceSubClass: Abstract Control Model */
        0x00,                                       /* bInterfaceProtocol: no protocol used */
        0x04,                                       /* Function string descriptor index */

            /* 1st Communications Interface */
            /*Interface 0, Alternate Setting 0, CCI Descriptor*/
            USB_INTERFACE_DESC_SIZE,            /* bLength: 9 */
            USB_INTERFACE_DESCRIPTOR_TYPE,      /* bDescriptorType */
            USB_CDC_CIF_NUM_0,                  /* 0: interface number  */
            0x00,                               /* Alternate Setting */
            0x01,                               /* endpoint count */
            CDC_COMMUNICATION_INTERFACE_CLASS,  /* CCI class*/
            CDC_ABSTRACT_CONTROL_MODEL,         /* ACM */
            0x00,                               /* Protocol  */
            0x04,                               /* Interface */

                /*Header Functional Descriptor*/
                0x05,                               /* bLength: Endpoint Descriptor size: 5 */
                CDC_CS_INTERFACE,                   /* bDescriptorType: CS_INTERFACE */
                CDC_HEADER,                         /* bDescriptorSubtype: Header Func Desc */
                WBVAL(CDC_V1_10), /* 1.10 */        /* bcdCDC */

                /*Call Management Functional Descriptor*/
                0x05,                               /* bFunctionLength: 5 */
                CDC_CS_INTERFACE,                   /* bDescriptorType: CS_INTERFACE */
                CDC_CALL_MANAGEMENT,                /* bDescriptorSubtype: Call Management Func Desc */
                0x01,                               /* bmCapabilities: device handles call management */
                USB_CDC_DIF_NUM_0,                  /* 1: bDataInterface: CDC data IF ID */

                /*Abstract Control Management Functional Descriptor*/
                0x04,                               /* bFunctionLength: 4 */
                CDC_CS_INTERFACE,                   /* bDescriptorType: CS_INTERFACE */
                CDC_ABSTRACT_CONTROL_MANAGEMENT,    /* bDescriptorSubtype: Abstract Control Management desc */
                0x02,                               /* bmCapabilities: SET_LINE_CODING, GET_LINE_CODING, SET_CONTROL_LINE_STATE supported */

                /*Union Functional Descriptor*/
                0x05,                               /* bFunctionLength: 5 */
                CDC_CS_INTERFACE,                   /* bDescriptorType: CS_INTERFACE */
                CDC_UNION,                          /* 6: bDescriptorSubtype: Union func desc */
                USB_CDC_CIF_NUM_0,                  /* bMasterInterface: Communication class interface is master */
                USB_CDC_DIF_NUM_0,                  /* bSlaveInterface0: Data class interface is slave 0 */

                /*Endpoint 1 Descriptor*/           /* event notification (optional) */
                USB_ENDPOINT_DESC_SIZE,             /* bLength: 7 */
                USB_ENDPOINT_DESCRIPTOR_TYPE,       /* bDescriptorType */
                USB_CDC_INT_EP_0,                   /* 0x81: bEndpointAddress */
                USB_ENDPOINT_TYPE_INTERRUPT,        /* bmAttributes */
                WBVAL(0x0010),                      /* wMaxPacketSize */
                0x08,          /* 8ms */            /* bInterval */

            /* 1st Data Interface */
            /* Interface 1, Alternate Setting 0, Data class interface descriptor*/
            USB_INTERFACE_DESC_SIZE,            /* bLength: 9 */
            USB_INTERFACE_DESCRIPTOR_TYPE,      /* bDescriptorType */
            USB_CDC_DIF_NUM_0,                  /* bInterfaceNumber: Number of Interface */
            0x00,                               /* bAlternateSetting: no alternate setting */
            0x02,                               /* bNumEndpoints: two endpoints used */
            CDC_DATA_INTERFACE_CLASS,           /* bInterfaceClass: Data Interface Class */
            0x00,                               /* bInterfaceSubClass: no subclass available */
            0x00,                               /* bInterfaceProtocol: no protocol used */
            0x04,                               /* iInterface: */

                /* Endpoint, EP Bulk Out */
                USB_ENDPOINT_DESC_SIZE,             /* bLength: 7 */
                USB_ENDPOINT_DESCRIPTOR_TYPE,       /* bDescriptorType */
                USB_CDC_OUT_EP_0,                   /* 0x02: bEndpointAddress */
                USB_ENDPOINT_TYPE_BULK,             /* bmAttributes */
                WBVAL(64),                          /* wMaxPacketSize */
                0x00,                               /* bInterval: ignore for Bulk transfer */

                /* Endpoint, EP Bulk In */
                USB_ENDPOINT_DESC_SIZE,             /* bLength: 7 */
                USB_ENDPOINT_DESCRIPTOR_TYPE,       /* bDescriptorType */
                USB_CDC_IN_EP_0,                    /* 0x82: bEndpointAddress */
                USB_ENDPOINT_TYPE_BULK,             /* bmAttributes */
                WBVAL(64),                          /* wMaxPacketSize */
                0x00,                               /* bInterval: ignore for Bulk transfer */

        /* ###################################################################################################### */
        /* Second Interface Pair */
        /* Interface association descriptor IAD */
        USB_INTERFACE_ASSOCIATION_DESC_SIZE,        /* bLength: 8 */
        USB_INTERFACE_ASSOCIATION_DESCRIPTOR_TYPE,  /* bDescriptorType */
        0x02,                                       /* bInterfaceNumber: Number of Interface */
        0x02,                                       /* bAlternateSetting: Alternate setting */
        CDC_COMMUNICATION_INTERFACE_CLASS,          /* bInterfaceClass: Communication Interface Class */
        CDC_ABSTRACT_CONTROL_MODEL,                 /* bInterfaceSubClass: Abstract Control Model */
        0x00,                                       /* bInterfaceProtocol: no protocol used */
        0x04,                                       /* iInterface: */

            /* 2nd Communications Interface */
            /*Interface 2, Alterante Setting 0, CCI Descriptor*/
            USB_INTERFACE_DESC_SIZE,            /* bLength: 9 */
            USB_INTERFACE_DESCRIPTOR_TYPE,      /* bDescriptorType */
            USB_CDC_CIF_NUM_2,                  /* 2: interface number  */
            0x00,                               /* unknown */
            0x01,                               /* endpoint count */
            CDC_COMMUNICATION_INTERFACE_CLASS,  /* CCI class*/
            CDC_ABSTRACT_CONTROL_MODEL,         /* ACM */
            0x00,                               /* Protocol  */
            0x04,                               /* Interface */

                /*Header Functional Descriptor*/
                0x05,                               /* bLength: Endpoint Descriptor size */
                CDC_CS_INTERFACE,                   /* bDescriptorType: CS_INTERFACE */
                CDC_HEADER,                         /* bDescriptorSubtype: Header Func Desc */
                WBVAL(CDC_V1_10), /* 1.10 */        /* bcdCDC */

                /*Call Management Functional Descriptor*/
                0x05,                               /* bFunctionLength */
                CDC_CS_INTERFACE,                   /* bDescriptorType: CS_INTERFACE */
                CDC_CALL_MANAGEMENT,                /* bDescriptorSubtype: Call Management Func Desc */
                0x01,                               /* bmCapabilities: device handles call management */
                0x01,                               /* 1: bDataInterface: CDC data IF ID */ /* Indicates multiplexed commands are handled via data interface */

                /*Abstract Control Management Functional Descriptor*/
                0x04,                               /* bFunctionLength */
                CDC_CS_INTERFACE,                   /* bDescriptorType: CS_INTERFACE */
                CDC_ABSTRACT_CONTROL_MANAGEMENT,    /* bDescriptorSubtype: Abstract Control Management desc */
                0x02,                               /* bmCapabilities: SET_LINE_CODING, GET_LINE_CODING, SET_CONTROL_LINE_STATE supported */

                /*Union Functional Descriptor*/
                0x05,                               /* bFunctionLength */
                CDC_CS_INTERFACE,                   /* bDescriptorType: CS_INTERFACE */
                CDC_UNION,                          /* 6: bDescriptorSubtype: Union func desc */
                USB_CDC_CIF_NUM_2,                  /* 2: bMasterInterface: Communication class interface is master */
                USB_CDC_DIF_NUM_2,                  /* 3: bSlaveInterface0: Data class interface is slave 0 */

                /*Endpoint 1 Descriptor*/           /* event notification (optional) */
                USB_ENDPOINT_DESC_SIZE,             /* bLength: 7 */
                USB_ENDPOINT_DESCRIPTOR_TYPE,       /* bDescriptorType */
                USB_CDC_INT_EP_2,                   /* 0x83: bEndpointAddress */
                USB_ENDPOINT_TYPE_INTERRUPT,        /* bmAttributes */
                WBVAL(0x0010),                      /* wMaxPacketSize */
                0x08,          /* 8ms */            /* bInterval */

            /* 2nd Data Interface */
            /* Interface 3, Alternate Setting 0, Data class interface descriptor*/
            USB_INTERFACE_DESC_SIZE,            /* bLength: 9 */
            USB_INTERFACE_DESCRIPTOR_TYPE,      /* bDescriptorType */
            USB_CDC_DIF_NUM_2,                  /* bInterfaceNumber: Number of Interface */
            0x00,                               /* bAlternateSetting: no alternate setting */
            0x02,                               /* bNumEndpoints: two endpoints used */
            CDC_DATA_INTERFACE_CLASS,           /* bInterfaceClass: Data Interface Class */
            0x00,                               /* bInterfaceSubClass: no subclass available */
            0x00,                               /* bInterfaceProtocol: no protocol used */
            0x04,                               /* iInterface: */

                /* Endpoint, EP Bulk Out */
                USB_ENDPOINT_DESC_SIZE,             /* bLength: 7 */
                USB_ENDPOINT_DESCRIPTOR_TYPE,       /* bDescriptorType */
                USB_CDC_OUT_EP_2,                   /* 0x04: bEndpointAddress */
                USB_ENDPOINT_TYPE_BULK,             /* bmAttributes */
                WBVAL(64),                          /* wMaxPacketSize */
                0x00,                               /* bInterval: ignore for Bulk transfer */

                /* Endpoint, EP Bulk In */
                USB_ENDPOINT_DESC_SIZE,             /* bLength: 7 */
                USB_ENDPOINT_DESCRIPTOR_TYPE,       /* bDescriptorType */
                USB_CDC_IN_EP_2,                    /* 0x84: bEndpointAddress */
                USB_ENDPOINT_TYPE_BULK,             /* bmAttributes */
                WBVAL(64),                          /* wMaxPacketSize */
                0x00,                               /* bInterval: ignore for Bulk transfer */

        /* ###################################################################################################### */
        /* Third Interface Pair */
        /* Interface association descriptor IAD */
        USB_INTERFACE_ASSOCIATION_DESC_SIZE,        /* bLength: 8 */
        USB_INTERFACE_ASSOCIATION_DESCRIPTOR_TYPE,  /* bDescriptorType */
        USB_CDC_CIF_NUM_3,                          /* bInterfaceNumber: Number of Interface: 0 */ /* The first interface number associated with this function */
        0x02,                                       /* The number of contiguous interfaces associated with this function */
        CDC_COMMUNICATION_INTERFACE_CLASS,          /* bInterfaceClass: Communication Interface Class */
        CDC_ABSTRACT_CONTROL_MODEL,                 /* bInterfaceSubClass: Abstract Control Model */
        0x00,                                       /* bInterfaceProtocol: no protocol used */
        0x04,                                       /* Function string descriptor index */

            /* 3rd Communications Interface */
            /*Interface 0, Alternate Setting 0, CCI Descriptor*/
            USB_INTERFACE_DESC_SIZE,            /* bLength: 9 */
            USB_INTERFACE_DESCRIPTOR_TYPE,      /* bDescriptorType */
            USB_CDC_CIF_NUM_3,                  /* 0: interface number  */
            0x00,                               /* Alternate Setting */
            0x01,                               /* endpoint count */
            CDC_COMMUNICATION_INTERFACE_CLASS,  /* CCI class*/
            CDC_ABSTRACT_CONTROL_MODEL,         /* ACM */
            0x00,                               /* Protocol  */
            0x04,                               /* Interface */

                /*Header Functional Descriptor*/
                0x05,                               /* bLength: Endpoint Descriptor size: 5 */
                CDC_CS_INTERFACE,                   /* bDescriptorType: CS_INTERFACE */
                CDC_HEADER,                         /* bDescriptorSubtype: Header Func Desc */
                WBVAL(CDC_V1_10), /* 1.10 */        /* bcdCDC */

                /*Call Management Functional Descriptor*/
                0x05,                               /* bFunctionLength: 5 */
                CDC_CS_INTERFACE,                   /* bDescriptorType: CS_INTERFACE */
                CDC_CALL_MANAGEMENT,                /* bDescriptorSubtype: Call Management Func Desc */
                0x01,                               /* bmCapabilities: device handles call management */
                USB_CDC_DIF_NUM_3,                  /* 1: bDataInterface: CDC data IF ID */

                /*Abstract Control Management Functional Descriptor*/
                0x04,                               /* bFunctionLength: 4 */
                CDC_CS_INTERFACE,                   /* bDescriptorType: CS_INTERFACE */
                CDC_ABSTRACT_CONTROL_MANAGEMENT,    /* bDescriptorSubtype: Abstract Control Management desc */
                0x02,                               /* bmCapabilities: SET_LINE_CODING, GET_LINE_CODING, SET_CONTROL_LINE_STATE supported */

                /*Union Functional Descriptor*/
                0x05,                               /* bFunctionLength: 5 */
                CDC_CS_INTERFACE,                   /* bDescriptorType: CS_INTERFACE */
                CDC_UNION,                          /* 6: bDescriptorSubtype: Union func desc */
                USB_CDC_CIF_NUM_3,                  /* bMasterInterface: Communication class interface is master */
                USB_CDC_DIF_NUM_3,                  /* bSlaveInterface0: Data class interface is slave 0 */

                /*Endpoint 1 Descriptor*/           /* event notification (optional) */
                USB_ENDPOINT_DESC_SIZE,             /* bLength: 7 */
                USB_ENDPOINT_DESCRIPTOR_TYPE,       /* bDescriptorType */
                USB_CDC_INT_EP_3,                   /* 0x85: bEndpointAddress */
                USB_ENDPOINT_TYPE_INTERRUPT,        /* bmAttributes */
                WBVAL(0x0010),                      /* wMaxPacketSize */
                0x08,          /* 8ms */            /* bInterval */

            /* 3rd Data Interface */
            /* Interface 1, Alternate Setting 0, Data class interface descriptor*/
            USB_INTERFACE_DESC_SIZE,            /* bLength: 9 */
            USB_INTERFACE_DESCRIPTOR_TYPE,      /* bDescriptorType */
            USB_CDC_DIF_NUM_3,                  /* bInterfaceNumber: Number of Interface */
            0x00,                               /* bAlternateSetting: no alternate setting */
            0x02,                               /* bNumEndpoints: two endpoints used */
            CDC_DATA_INTERFACE_CLASS,           /* bInterfaceClass: Data Interface Class */
            0x00,                               /* bInterfaceSubClass: no subclass available */
            0x00,                               /* bInterfaceProtocol: no protocol used */
            0x04,                               /* iInterface: */

                /* Endpoint, EP Bulk Out */
                USB_ENDPOINT_DESC_SIZE,             /* bLength: 7 */
                USB_ENDPOINT_DESCRIPTOR_TYPE,       /* bDescriptorType */
                USB_CDC_OUT_EP_3,                   /* 0x06: bEndpointAddress */
                USB_ENDPOINT_TYPE_BULK,             /* bmAttributes */
                WBVAL(64),                          /* wMaxPacketSize */
                0x00,                               /* bInterval: ignore for Bulk transfer */

                /* Endpoint, EP Bulk In */
                USB_ENDPOINT_DESC_SIZE,             /* bLength: 7 */
                USB_ENDPOINT_DESCRIPTOR_TYPE,       /* bDescriptorType */
                USB_CDC_IN_EP_3,                    /* 0x86: bEndpointAddress */
                USB_ENDPOINT_TYPE_BULK,             /* bmAttributes */
                WBVAL(64),                          /* wMaxPacketSize */
                0x00,                               /* bInterval: ignore for Bulk transfer */

    /* Terminator */
    0                                  /* bLength */
};

 

ラベル(2)
0 件の賞賛
返信
1 返信

1,323件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @dean_sands 

1) First method is debug step by step check issue.

2)Recommend use Config tool inside MCUXpresso IDE to config. Can refer to:

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Using-ConfigTool-to-create-USB-Project-F....  

 

BR

Alice

0 件の賞賛
返信