LPC4088 with SPIFI FLASH Above 16MB/24 Bit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4088 with SPIFI FLASH Above 16MB/24 Bit

2,076件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by schibli on Fri Jan 09 06:03:07 MST 2015
Can LPC408x support more than 16MB of SPIFI SPI flash memory with the newest version of SPIFILIB (V1.01),
or is it a matter of hardware (24 Bit addressing limit, SPIFI Buffer Space 0x2800 0000 - 0x28FF FFFF)?

Thanks.
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,734件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Sat Jan 10 07:43:56 MST 2015
Hi schibli,
LPC4088 supports only up to 16MB SPIFI flash memory mapped area. LPC1800/4300 devices support more than 16MB SPIFI flash memory. SPIFI hardware supports more than 3 bytes addressing. It was not implemented in new SPIFI library. We will implement it. It has been implemented in old version of SPIFI library.
0 件の賞賛
返信

1,734件の閲覧回数
hungmai
Contributor I

Can SPIFI flash greater than 16MB be used in Command mode?

0 件の賞賛
返信

1,734件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

The software interface to the SPIFI controller is the same as for the LPC43xx parts so I can see no reason why this would not work - however I have not actually tried this.  Of course regardless, only 16MBs will be accessible from code running on the LPC4088.

Yours,

LPCXpresso-support

0 件の賞賛
返信