LPC4088 will support two Ethernet Subnets?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4088 will support two Ethernet Subnets?

1,706件の閲覧回数
avinashh
Contributor III

Hi,

The Ethernet port of LPC4088 can be assigned with two Subnets (like 192.168.1.1 and 192.168.2.1)?

Please confirm. 

-Avinash

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,593件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi  Avinash H ,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.

It's available to achieve your purpose, however I'd highly recommend you to use the LWIP or other TCP/IP stack for this implementation.

Have a great day,
TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
0 件の賞賛
返信