LPC4088 will support two Ethernet Subnets?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4088 will support two Ethernet Subnets?

1,749 次查看
avinashh
Contributor III

Hi,

The Ethernet port of LPC4088 can be assigned with two Subnets (like 192.168.1.1 and 192.168.2.1)?

Please confirm. 

-Avinash

标签 (2)
标记 (2)
0 项奖励
回复
1 回复

1,636 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi  Avinash H ,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.

It's available to achieve your purpose, however I'd highly recommend you to use the LWIP or other TCP/IP stack for this implementation.

Have a great day,
TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
0 项奖励
回复