LPC4088 sleep mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4088 sleep mode

1,287件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by an.skornyakov on Tue Jun 25 04:37:12 MST 2013

 Hi,


I have lpc4088 based device. I would like to use sleep mode, datasheet says I ought to set some value for SLEEPDEEP bit in Cortex-M4 System Control Register to select between Sleep and Deep Sleep mode. I couldn't find this System Control Register and those bit. Is System Control and Status register implied? 


Best regards,


Anton 

ラベル(1)
0 件の賞賛
返信
1 返信

1,201件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Thu Aug 29 15:46:00 MST 2013
Hi Anton,

The SLEEPDEEP bit can be set in the System Control Register (SCR) register which you can find in the sample code. You can find the sample code here :

http://www.lpcware.com/content/nxpfile/lpc407x-and-lpc408x-cmsis-compliant-standard-peripheral-firmw...

The information on the SCR register can be found in the ARM Cortex M4 Reference Guide : http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0439d/index.html .

Thanks,
SK
0 件の賞賛
返信