LPC4088 memory interface layout

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4088 memory interface layout

1,592 次查看
flavioalpino
Contributor I

Hello,

I need info about layout constraints between LPC4088 micro and an SDRAM dinamic RAM chip.

I would like to know how to trace address, controls and data lines, lines matching, impedence....

How can I get these info?

Could you suggest some application note or datasheet?

The memory I have to interface is an ISSI IS42S32800G working at about 133MHz.

Thank you very much

标签 (2)
0 项奖励
回复
1 回复

1,396 次查看
soledad
NXP Employee
NXP Employee

Hello Flavio,

Please check the below application notes.

http://www.nxp.com/documents/application_note/AN11508.pdf

http://www.nxp.com/documents/application_note/AN10935.pdf


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复