LPC4088 memory interface layout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4088 memory interface layout

1,625件の閲覧回数
flavioalpino
Contributor I

Hello,

I need info about layout constraints between LPC4088 micro and an SDRAM dinamic RAM chip.

I would like to know how to trace address, controls and data lines, lines matching, impedence....

How can I get these info?

Could you suggest some application note or datasheet?

The memory I have to interface is an ISSI IS42S32800G working at about 133MHz.

Thank you very much

ラベル(2)
0 件の賞賛
返信
1 返信

1,429件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Flavio,

Please check the below application notes.

http://www.nxp.com/documents/application_note/AN11508.pdf

http://www.nxp.com/documents/application_note/AN10935.pdf


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信