LPC4088 and TFTs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4088 and TFTs

873 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mulfycrowh on Sun Jan 17 07:58:14 MST 2016
Hi everyone !

I am using LPC4088.
The question is about hardware development and more precisely how to select the pins of the LPC4088.
EMC pins are used in my development for external flash and sram.
I would like to add a LCD screen 24 bits.
The idea is to use LCD_VD[0...23] pins. I noticed that all these pins are declared in the datasheet as outputs except LCD_VD[3] and LCD_VD[7] that are inputs on pin P2.9.
Why inputs ? Is there a mistake in the datasheet ?
Data bus for TFTs is made of outputs.
Can I use P2.9 as an output for LCD purpose ?

Many thanks for help
Labels (1)
0 Kudos
Reply
0 Replies