LPC4088 USB-OTG External Transceiver required?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4088 USB-OTG External Transceiver required?

2,561件の閲覧回数
amitkolekar
Contributor I

Hi,

I want to implement USB OTG on LPC4088. In user manual for OTG functionality external OTG transceiver(ISP1302) is used. LPC4088 has OTG controller. 

Is it necessary to use external transceiver for OTG functionality?

0 件の賞賛
返信
2 返答(返信)

2,080件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi Amit,

Yes, for full OTG compliant it is necessary to add externally the OTG transceiver (ISP1302). This is in order to manage the pins Vbus & ID in addition to control "on the fly" the Host or Device stack.


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,080件の閲覧回数
priyankb
Contributor III

Hi soledad‌,

If I want to use the same USB port as a device & as a host when connected to PC or when pendrive is connected to board respectively, do I necessarily need to use USB transceiver for this purpose?

I will not switch host & device without detaching the the USB(device/host). So if I put my board in device mode(default configuration) & when another device is attached ID level will trigger interrupt & then I will initialize board as host by removing pull up, adding pull downs, & applying VBUS(using switches & charge pump). Again when device is detached I will reinitialize it to device by removing pull downs, VBUS, & adding pull up. Will this work?

Thank you.

Priyank.

0 件の賞賛
返信