LPC4088 QSB + LPCXPRESSO V8.2.2 + LPCLINK2 error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4088 QSB + LPCXPRESSO V8.2.2 + LPCLINK2 error

1,351件の閲覧回数
pascalreygner
Contributor II

the LPC4088 QSB card is working correctly when using mbedCompiler (programming software / reset / soft working correctly).

when i connect EmbeddedArtists LPC4088 QSB Card + LPCXPRESSO V8.2.2 + LPCLINK2, the following failure appears on console debug message when trying connection with debugger : 

" LPCXpresso RedlinkMulti Driver v8.2 (Sep 5 2016 10:12:38 - crt_emu_cm_redlink build 725)
Found chip XML file in C:/Users/preyg/Documents/LPCXpresso_8.2.2_650/workspace/lwip_tcpecho_freertos/Debug/LPC4088.xml
Failed on connect: Ee(36). Could not connect to core.
No connection to emulator device ".

ERROR REPORTED BY TARGET : 

02: Failed on connect
Could not connect to core.
31: No connection to emulator device

i have tried proposed solution on this blog : Regaining debug access to target MCU 

using buttons SW1 + SW2 or changing  "vector cache", it is still don't work

DO YOU HAVE ANY SOLUTION?

thanks a lot

0 件の賞賛
返信
1 返信

1,211件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

I have posted a response into the duplicate thread you created - https://community.nxp.com/thread/447904#comment-891419 

I suggest posting any further information into that thread (and closing this thread if possible).

Regards,

LPCXpresso Support.

0 件の賞賛
返信