LPC4088 - IO configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4088 - IO configuration

1,104 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TKoe on Tue Mar 26 02:54:52 MST 2013
Hello!

I've been reading the user manual for the 4088 and I've found some error in the part with the IO configuration.
On page 141 all type W pins are listed: P0[7] to P0[9], P1[5] to P1[7], P[1]14 and P[1]16 to P[1]17.
However, on page 140 only the pins on Port 0 are listed. The other pins are also not listed on page 130 (the pins that are not type D pins). They are also missing in the type D table.

I am assuming that that is a copy/paste error from the LPC1788 and that the tables for the type D and W pins are correct (and only the descriptions are faulty) but can anyone confirm that?

Best Regards!
Labels (1)
0 Kudos
Reply
1 Reply

1,053 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Fri Aug 30 14:46:43 MST 2013
Hi, TKoe,
You are correct!
Next UM release will have this fixed.
regard,
0 Kudos
Reply